FS6510 Level Triggering at low level

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

FS6510 Level Triggering at low level

跳至解决方案
2,375 次查看
N123
Contributor II

Hi,

Is it possible configure a low-level trigger on IO of FS6510 SBC for waking up?

We want to use level triggering but below a voltage.

For example, whenever IO5 receives a level lower than 5V, then it should wake up the system. (We don’t want to depend on edge triggering as we are unsure on rate of falling).

In case there is some documentation stating all register definitions, please share.

0 项奖励
回复
1 解答
2,351 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Neetigya,

I do not have such data. I can only add an info about the deglitch time:

Deglitch.JPG

Meaning, if IO voltage < 2.1V and the duration is > 70us, then the device will wake up. 

Best regards,

Tomas

在原帖中查看解决方案

0 项奖励
回复
4 回复数
2,364 次查看
N123
Contributor II

Hi,

Thank you. Could you please share edge triggered data similar way? Like voltage levels and rate of rise and fall (as in 2nd screenshot)? 

 

0 项奖励
回复
2,352 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Neetigya,

I do not have such data. I can only add an info about the deglitch time:

Deglitch.JPG

Meaning, if IO voltage < 2.1V and the duration is > 70us, then the device will wake up. 

Best regards,

Tomas

0 项奖励
回复
2,348 次查看
N123
Contributor II

Hi, Thank you very much.

We were asking regarding this time constraint only.

0 项奖励
回复
2,367 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Neetigya,

Yes, it is possible to achieve that by setting WU_IO5_1:0 bits to 0b10:

WU.JPG

Valid high/low voltage: IO5 pin Voltage>2.6V = High, Voltage<2.1V = Low:

Digital Input.JPG

Best regards,

Tomas

0 项奖励
回复