FS6510 Level Triggering at low level

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FS6510 Level Triggering at low level

ソリューションへジャンプ
2,362件の閲覧回数
N123
Contributor II

Hi,

Is it possible configure a low-level trigger on IO of FS6510 SBC for waking up?

We want to use level triggering but below a voltage.

For example, whenever IO5 receives a level lower than 5V, then it should wake up the system. (We don’t want to depend on edge triggering as we are unsure on rate of falling).

In case there is some documentation stating all register definitions, please share.

0 件の賞賛
返信
1 解決策
2,338件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Neetigya,

I do not have such data. I can only add an info about the deglitch time:

Deglitch.JPG

Meaning, if IO voltage < 2.1V and the duration is > 70us, then the device will wake up. 

Best regards,

Tomas

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,351件の閲覧回数
N123
Contributor II

Hi,

Thank you. Could you please share edge triggered data similar way? Like voltage levels and rate of rise and fall (as in 2nd screenshot)? 

 

0 件の賞賛
返信
2,339件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Neetigya,

I do not have such data. I can only add an info about the deglitch time:

Deglitch.JPG

Meaning, if IO voltage < 2.1V and the duration is > 70us, then the device will wake up. 

Best regards,

Tomas

0 件の賞賛
返信
2,335件の閲覧回数
N123
Contributor II

Hi, Thank you very much.

We were asking regarding this time constraint only.

0 件の賞賛
返信
2,354件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Neetigya,

Yes, it is possible to achieve that by setting WU_IO5_1:0 bits to 0b10:

WU.JPG

Valid high/low voltage: IO5 pin Voltage>2.6V = High, Voltage<2.1V = Low:

Digital Input.JPG

Best regards,

Tomas

0 件の賞賛
返信