FRDM33772CSPEVB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,898件の閲覧回数
hajianik
Senior Contributor I

Hi,

I have a FRDM33772CSPEVB for battery acquisition system. This board accts as an slave to my Microcontroller(S32K311) Master, I DO HAVE A Q100 EVAL board for the latter.

 

I can connect the the 37722c evb right on the top of the q100(s32k3), The pins match.

using this way ,would I have all the relevant connections between the Master and slave? or I need to wire them up manually?

 

Thanks,

タグ(1)
0 件の賞賛
返信
1 解決策
2,724件の閲覧回数
diazmarin09
NXP TechSupport
NXP TechSupport

Hello hajianik,

Please accept my apologies for the delayed response.

Do you mean the S32K312EVB-Q172 board?

Regards,

David

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,830件の閲覧回数
diazmarin09
NXP TechSupport
NXP TechSupport

Hello hajianik,

I hope all is great with you. Thank you for using the NXP communities.

The board is designed to be fully compatible with the S32K144EVB board.

Could you please specify the board that you have? I do recommend comparing the pinout of both evaluation boards to confirm its compatibility.

I hope this information helps.

Regards,

David

0 件の賞賛
返信
2,821件の閲覧回数
hajianik
Senior Contributor I
Hi
the board is :XS32K31XEVB-Q100.
Thanks,
0 件の賞賛
返信
2,725件の閲覧回数
diazmarin09
NXP TechSupport
NXP TechSupport

Hello hajianik,

Please accept my apologies for the delayed response.

Do you mean the S32K312EVB-Q172 board?

Regards,

David

0 件の賞賛
返信
2,721件の閲覧回数
hajianik
Senior Contributor I
Hi,
No, It is : XS32K31XEVB-Q100.
Lets just forget this. It is not important anymore.
Thanks.
0 件の賞賛
返信