FRDM33772CSPEVB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FRDM33772CSPEVB

Jump to solution
2,931 Views
hajianik
Senior Contributor I

Hi,

I have a FRDM33772CSPEVB for battery acquisition system. This board accts as an slave to my Microcontroller(S32K311) Master, I DO HAVE A Q100 EVAL board for the latter.

 

I can connect the the 37722c evb right on the top of the q100(s32k3), The pins match.

using this way ,would I have all the relevant connections between the Master and slave? or I need to wire them up manually?

 

Thanks,

Tags (1)
0 Kudos
Reply
1 Solution
2,757 Views
diazmarin09
NXP TechSupport
NXP TechSupport

Hello hajianik,

Please accept my apologies for the delayed response.

Do you mean the S32K312EVB-Q172 board?

Regards,

David

View solution in original post

0 Kudos
Reply
4 Replies
2,863 Views
diazmarin09
NXP TechSupport
NXP TechSupport

Hello hajianik,

I hope all is great with you. Thank you for using the NXP communities.

The board is designed to be fully compatible with the S32K144EVB board.

Could you please specify the board that you have? I do recommend comparing the pinout of both evaluation boards to confirm its compatibility.

I hope this information helps.

Regards,

David

0 Kudos
Reply
2,854 Views
hajianik
Senior Contributor I
Hi
the board is :XS32K31XEVB-Q100.
Thanks,
0 Kudos
Reply
2,758 Views
diazmarin09
NXP TechSupport
NXP TechSupport

Hello hajianik,

Please accept my apologies for the delayed response.

Do you mean the S32K312EVB-Q172 board?

Regards,

David

0 Kudos
Reply
2,754 Views
hajianik
Senior Contributor I
Hi,
No, It is : XS32K31XEVB-Q100.
Lets just forget this. It is not important anymore.
Thanks.
0 Kudos
Reply