Extract firmware

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Extract firmware

2,169件の閲覧回数
KhangVA
Contributor I

Dear all, 

I wanna extract firmware from MK60FN1M0VLQ12. But I can not find solution. 
Can anyone help me. Thanks all!

0 件の賞賛
返信
3 返答(返信)

2,126件の閲覧回数
PabloAvalos
NXP TechSupport
NXP TechSupport

Hi @KhangVA 

 

Thank you so much for using our community, and thanks a lot for your patience. We have some backlog on the requests.

 

Regarding what you are asking for, if that mcu is bricked or has the firmware assured you won't be able to extract the firmware from that, otherwise, if chip is new and it is yours, please let me know which debugger and software you are using for so I could help you.

 

Please let me know any update and your comments. Of course if you have more questions, I will be more than happy to assist you.

 

Thank you in advance.
Best Regards.
Pablo Avalos.

0 件の賞賛
返信

2,089件の閲覧回数
KhangVA
Contributor I

Dear, 

Chip on board still active and run as picture below.z3531732940676_5f2e8bc2b71c60720add866d29b1a009.jpg

0 件の賞賛
返信

2,086件の閲覧回数
PabloAvalos
NXP TechSupport
NXP TechSupport

Hi @KhangVA 

 

Thanks for sharing.

 

In order to help you, may I know which debug interface and software you are using to extract the firmware from your chip? And as I see, you are using a custom board, so please I would like to suggest you to check very well your hardware to be able to flash and extract firmware from your mcu.

 

Please let me know if you have more questions.

 

Best Regards.
Pablo Avalos.

0 件の賞賛
返信