Ethernet throughput using LWIP + FreeRTOS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Ethernet throughput using LWIP + FreeRTOS

1,296 Views
mayoor_p
Contributor I

I am testing the ethernet throughput of NxP LPC54018 MCU on OM40003 development board and observing poor throughput.

Environment details:
Tool: MCUXpresso v 11.0.0 build Id 2516

Project details:
Selected MCU LPC54018
Target board not selected
Selected Device package: LPC54018JET180
Operating System: Amazon-FreeRTOS (10.2.0)
Drivers: lpc_enet (2.1.3) in addition to other auto select drivers.
CMSIS Drivers: None
Utilities: None
Middleware: LwIP TCPIP Networking Stack (2.1.2)
Board Components: phylan8720a(1.0.0)
Abstraction Layer: None
Software ComponentsL None
Library Type(and hosting variant): Redlib(none)

With the above settings of the project and referring SDK example project "lpcxpresso54018_lwip_ping_freertos" I created application which sends ICMP ping echo to a target IP address using lwip_sendto( ) API in while loop.

The time taken for lwip_sendto() to execute and come out for next call in loop is more than 20 milliseconds as can be seen from wireshark logs in the screenshot and also when I measured using timer.

Any suggestions on what settings are required for achieving best througput?

With Regards
MayoorLPC54018 ethernet throughput_001.png

0 Kudos
Reply
1 Reply

1,226 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Mayoor,

As you know that the Ethernet is bus architecture, all nodes have the same priority, each node uses Carrier-sense multiple access with collision detection method to access Ethernet, I do not think there is method to increase the througput via software configuration.

Hope it can help you

BR

XiangJun Rong

0 Kudos
Reply