Error while running the example code of the NFC Reader Library on a raspberry pi and CLRC633

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error while running the example code of the NFC Reader Library on a raspberry pi and CLRC633

1,228件の閲覧回数
iuliacornea
Contributor I

Hello everyone!

I just started working with the CLRC633, connected to a raspberry pi zero W.

I followed the instructions from the Linux Installation manual and all enabled spi on my raspberry pi.

However, when I am running the first example code (NfcrdlibEx1_BasicDiscoveryLoop) from the NFC Reader Library, I get the following errors:

" Line: 570 Error - (0x0204) has occurred : 0xCCEE CC-Component ID, EE-Error code. Refer-ph_Status.h
Line: 210 Error - (0x0204) has occurred : 0xCCEE CC-Component ID, EE-Error code. Refer-ph_Status.h"

Does anyone know what the 0x0204 error represents and how it can be fixed?

Thank you in advance!

 

0 件の賞賛
返信
0 返答(返信)