How to enable Egress timestamping on specific port of switch ?
As per user manual UM11040 section 6.1.1.5 PTP Egress Timestamping, we can read timestamp values. But is there any register/table which can be used to enable timestamping.
Timestamping is controlled by TAKETS and TSREG fields L2 Address Lookup Table. See UM11040, Table 16 for details.
How to enable or disable a pre-configured VLAN on specific port of switch ?
As per user manual UM11040 Table 3 entry, VLAN Lookup table – by default VLAN 0 is enabled. Is there any register/table that can be modified to enable/disable VLAN for specific port.
Refer to AH1704, Section 6.6.2, UM11040, Sections 5.2.7 and 5.2.5 for configuring VLANs
Hope this helps,
Platon