imx28 linux 2.6.35.XX sja1105

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx28 linux 2.6.35.XX sja1105

769 Views
shashikanthirem
Contributor III

Hi All,

i am seeing a sja1105 driver for linux 4.0 kernel but since our product is based on linux 2.6.35.xx kernel, need this switch over spi there, if any one face this  issue, please share the code file either user level/ driver level 

0 Kudos
4 Replies

575 Views
igorpadykov
NXP Employee
NXP Employee

Hi shashikant

one can try linux-fslc kernels where it is supported:

GitHub - Freescale/linux-fslc: Linux kernel source tree 

GitHub - Freescale/meta-freescale at morty 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

575 Views
shashikanthirem
Contributor III

Thanks igor,, but we are using ltib as a  build rootfs but not yocto, it it was yocto then we would easily get the things move on easily, but this is outdated product with an new eth switch has been integrated , where i am finding difficult to map the driver for LTIB/  which has kernel 2.6.35.abc version. if i get overview of simple application sja1105 code file also fine which shall be able to build on 2.6 linux kernel

any input further.

0 Kudos

575 Views
igorpadykov
NXP Employee
NXP Employee

Hi shashikant

nxp has special service for software customization

Commercial Support and Engineering Services | NXP 

Best regards
igor

0 Kudos

575 Views
shashikanthirem
Contributor III

Thanks igor,, but we are using ltib as a  build rootfs but not yocto, it it was yocto then we would easily get the things move on easily, but this is outdated product with an new eth switch has been integrated , where i am finding difficult to map the driver for LTIB/  which has kernel 2.6.35.abc version. if i get overview of simple application sja1105 code file also fine which shall be able to build on 2.6 linux kernel

0 Kudos