EB tresos issue - module cannot be installed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

EB tresos issue - module cannot be installed

3,292 Views
Yang_C
Contributor IV

Hi all,

I have a problem with EB tresos, hope someone can give some hints. Thank you in advance.

I want to open a project on EB, the EB version i am using is 27.1.0. When I tried to open the module, an error pop up as below, it says Eth_43_PFE_TS_T40D11M12I0R0 is not installed:

error.png

I understanding when installing the EB tresos, I should link to the RTD folder, I indeed did:

link.png

Besides, I also cope paste the Eth_43_PFE_TS_T40D11M12I0R0 to RTD folder and EB plugins folder:

RTD folder.png

tresos folder.png

All the above actions make no difference, the error stays.

Do I miss some setup? 

 

BR,

Yang

0 Kudos
Reply
7 Replies

3,225 Views
alejandro_e
NXP TechSupport
NXP TechSupport

Hello @Yang_C,

Sorry for the late reply. everything seems to be correct as you mentioned. Please help me with the following test:

  • Can you try opening one of the examples present in the PFE-DRV_S32G_M7_MCAL_1.2.0.\example_application folder? to check if you can open those projects without problems.
  • Remove the link file and use only the copied plugins in the Tresos directory. The S32G MCAL Driver Release Notes for version 1.2.0 mention the installation methods as mutually exclusive:
    • alejandro_e_0-1765490795933.png

       

Let me know if you can open the example projects or if removing the link file changes de behavior for your project.

 

Thanks

0 Kudos
Reply

3,217 Views
Yang_C
Contributor IV

Hi alejandro_e,

Thank you for your reply.

 

Let me answer the result one by one.

  • Can you try opening one of the examples present in the PFE-DRV_S32G_M7_MCAL_1.2.0.\example_application folder? to check if you can open those projects without problems.

  - Tried, didn't work, still the Eth module not installed

  • Remove the link file and use only the copied plugins in the Tresos directory. 

  - Tried, didn't work, still the Eth module not installed

 

I also downloaded PFE-DRV_S32G_M7_MCAL_1.4.0 and tried opening one of the example projects in PFE-DRV_S32G_M7_MCAL_1.4.0, it works, either the Eth module is in NXP/RTD folder or in EB/tresos/plugins folder, both ways can open the project without any problems.

 

BR,

Yang

0 Kudos
Reply

3,054 Views
alejandro_e
NXP TechSupport
NXP TechSupport

Hello @Yang_C,

Sorry for the late reply. I tried to reproduce the issue on my side, however I was not able to do so. I copied the plugins and created the link file, I also copied the two PFE drivers versions you are using, 1.2.0 and 1.4.0. Can you run the following powershell command in C:\EB\tresos27\plugins andC:\NXP\SW32G_RTD_4.4_4.0.2_HF03\eclipse\plugins:

> Get-ChildItem -Depth 0

 

Here is the output from my setup:

PS C:\EB\tresos27\plugins> Get-ChildItem -Depth 0


    Directory: C:\EB\tresos27\plugins


Mode                 LastWriteTime         Length Name
----                 -------------         ------ ----
d-----     15/12/2025  02:23 p. m.                Adc_TS_T40D11M40I2R0
d-----     15/12/2025  02:24 p. m.                BaseNXP_TS_T40D11M40I2R0
d-----     15/12/2025  02:24 p. m.                CanIf_TS_T40D11M40I2R0
d-----     15/12/2025  02:24 p. m.                Can_TS_T40D11M40I2R0
d-----     15/12/2025  02:24 p. m.                Crc_TS_T40D11M40I2R0
d-----     15/12/2025  02:24 p. m.                CryIf_TS_T40D11M40I2R0
d-----     15/12/2025  02:24 p. m.                Crypto_TS_T40D11M40I2R0
d-----     15/12/2025  02:24 p. m.                Csm_TS_T40D11M40I2R0
d-----     15/12/2025  02:24 p. m.                Dem_TS_T40D11M40I2R0
d-----     15/12/2025  02:24 p. m.                Det_TS_T40D11M40I2R0
d-----     15/12/2025  02:24 p. m.                Dio_TS_T40D11M40I2R0
d-----     30/01/2025  04:42 p. m.                dreisoft.tresos.fibeximporter
d-----     30/01/2025  04:42 p. m.                dreisoft.tresos.generator.ng.api
d-----     15/12/2025  02:24 p. m.                EcuC_TS_T40D11M40I2R0
d-----     15/12/2025  02:24 p. m.                EcuM_TS_T40D11M40I2R0
d-----     15/12/2025  02:24 p. m.                Eep_TS_T40D11M40I2R0
d-----     15/12/2025  02:24 p. m.                EthIf_TS_T40D11M40I2R0
d-----     15/12/2025  02:24 p. m.                EthSwt_TS_T40D11M40I2R0
d-----     15/12/2025  02:24 p. m.                EthTrcv_TS_T40D11M40I2R0
d-----     15/12/2025  02:35 p. m.                Eth_43_PFE_TS_T40D11M12I0R0
d-----     15/12/2025  03:04 p. m.                Eth_43_PFE_TS_T40D11M14I0R0
d-----     15/12/2025  02:24 p. m.                Eth_TS_T40D11M40I2R0
d-----     15/12/2025  02:24 p. m.                Fee_TS_T40D11M40I2R0
d-----     15/12/2025  02:24 p. m.                Fls_TS_T40D11M40I2R0
d-----     15/12/2025  02:24 p. m.                FrIf_TS_T40D11M40I2R0
d-----     15/12/2025  02:24 p. m.                Fr_TS_T40D11M40I2R0
d-----     15/12/2025  02:24 p. m.                Gpt_TS_T40D11M40I2R0
d-----     15/12/2025  02:24 p. m.                I2c_TS_T40D11M40I2R0
d-----     15/12/2025  02:24 p. m.                Icu_TS_T40D11M40I2R0
d-----     15/12/2025  02:24 p. m.                LinIf_TS_T40D11M40I2R0
d-----     15/12/2025  02:24 p. m.                Lin_TS_T40D11M40I2R0
d-----     15/12/2025  02:24 p. m.                Mcl_TS_T40D11M40I2R0
d-----     15/12/2025  02:24 p. m.                Mcu_TS_T40D11M40I2R0
d-----     15/12/2025  02:24 p. m.                MemIf_TS_T40D11M40I2R0
d-----     15/12/2025  02:24 p. m.                Ocotp_TS_T40D11M40I2R0
d-----     15/12/2025  02:24 p. m.                Ocu_TS_T40D11M40I2R0
d-----     30/01/2025  04:42 p. m.                org.apache.ant_1.9.6.v201510161327
d-----     30/01/2025  04:42 p. m.                org.eclipse.equinox.launcher.gtk.linux.x86_64_1.1.401.v20161122-1740
d-----     30/01/2025  04:42 p. m.                org.eclipse.equinox.launcher.win32.win32.x86_64_1.1.401.v20161122-1740
d-----     30/01/2025  04:42 p. m.                org.eclipse.jdt.debug_3.10.1.v20160811-0441
d-----     30/01/2025  04:42 p. m.                org.eclipse.pde.build_3.9.200.v20160204-0642
d-----     30/01/2025  04:42 p. m.                org.eclipse.ui.themes_1.1.300.v20161107-1827
d-----     15/12/2025  02:24 p. m.                Os_TS_T40D11M40I2R0
d-----     15/12/2025  02:24 p. m.                Pcie_TS_T40D11M40I2R0
d-----     15/12/2025  02:24 p. m.                Platform_TS_T40D11M40I2R0
d-----     15/12/2025  02:24 p. m.                Pmic_TS_T40D11M40I2R0
d-----     15/12/2025  02:24 p. m.                Port_TS_T40D11M40I2R0
d-----     15/12/2025  02:24 p. m.                Pwm_TS_T40D11M40I2R0
d-----     15/12/2025  02:24 p. m.                Qdec_TS_T40D11M40I2R0
d-----     15/12/2025  02:24 p. m.                Resource_TS_T40D11M40I2R0
d-----     15/12/2025  02:24 p. m.                Rm_TS_T40D11M40I2R0
d-----     15/12/2025  02:24 p. m.                Rte_TS_T40D11M40I2R0
d-----     15/12/2025  02:24 p. m.                Serdes_TS_T40D11M40I2R0
d-----     15/12/2025  02:24 p. m.                Spi_TS_T40D11M40I2R0
d-----     15/12/2025  02:24 p. m.                Thermal_TS_T40D11M40I2R0
d-----     15/12/2025  02:23 p. m.                Uart_TS_T40D11M40I2R0
d-----     15/12/2025  02:23 p. m.                WdgIf_TS_T40D11M40I2R0
d-----     15/12/2025  02:23 p. m.                Wdg_43_VR5510_TS_T40D11M40I2R0
d-----     15/12/2025  02:23 p. m.                Wdg_TS_T40D11M40I2R0
-a----     25/06/2020  10:09 a. m.         466201 com.collabnet.subversion.merge_3.0.12.jar
-a----     22/08/2024  10:06 a. m.           2746 com.freescale.tools.tresos.xpath.jar
-a----     25/06/2020  10:09 a. m.       11365876 com.ibm.icu_56.1.0.v201601250100.jar
-a----     25/06/2020  10:09 a. m.         301911 com.jcraft.jsch_0.1.53.v201508180515.jar
-a----     22/08/2024  10:23 a. m.           1757 com.nxp.tools.tresos.xpath.sqrt.jar
-a----     25/06/2020  10:09 a. m.          69600 dreisoft.tresos.application.core.jar
-a----     25/06/2020  10:09 a. m.        1203946 dreisoft.tresos.application.launcher2.jar
-a----     25/06/2020  10:09 a. m.          33385 dreisoft.tresos.autosar2.api.jar
-a----     25/06/2020  10:09 a. m.         258839 dreisoft.tresos.autosar2.jar
-a----     25/06/2020  10:09 a. m.       18350433 dreisoft.tresos.autosar2.parser.jar
-a----     25/06/2020  10:09 a. m.          90003 dreisoft.tresos.autosarimexporter.jar
-a----     25/06/2020  10:09 a. m.         120522 dreisoft.tresos.comimporter.api.jar
-a----     25/06/2020  10:09 a. m.          20061 dreisoft.tresos.comimporter.hooks.api.jar
-a----     25/06/2020  10:09 a. m.         100263 dreisoft.tresos.comimporter.jar
-a----     25/06/2020  10:09 a. m.        1967950 dreisoft.tresos.core.jar
-a----     25/06/2020  10:09 a. m.          21721 dreisoft.tresos.customization.jar
-a----     25/06/2020  10:09 a. m.         227643 dreisoft.tresos.datamodel2.api.jar
-a----     25/06/2020  10:09 a. m.        3963165 dreisoft.tresos.datamodel2.jar
-a----     25/06/2020  10:09 a. m.         236687 dreisoft.tresos.datamodeldiffer.jar
-a----     25/06/2020  10:09 a. m.         147890 dreisoft.tresos.dbcimporter.jar
-a----     25/06/2020  10:09 a. m.           1291 dreisoft.tresos.doc.eclipse.reference.jar
-a----     25/06/2020  10:09 a. m.        2444638 dreisoft.tresos.formulalanguage.parser.jar
-a----     25/06/2020  10:09 a. m.          49013 dreisoft.tresos.generator.api.jar
-a----     25/06/2020  10:09 a. m.        1153378 dreisoft.tresos.guidedconfig.api.jar
-a----     25/06/2020  10:09 a. m.       14012053 dreisoft.tresos.help.api.jar
-a----     25/06/2020  10:09 a. m.          64742 dreisoft.tresos.launcher2.api.jar
-a----     25/06/2020  10:09 a. m.        8040376 dreisoft.tresos.launcher2.jar
-a----     25/06/2020  10:09 a. m.         147897 dreisoft.tresos.ldfimporter.jar
-a----     25/06/2020  10:09 a. m.          26974 dreisoft.tresos.lib2.api.jar
-a----     25/06/2020  10:09 a. m.        7555679 dreisoft.tresos.lib2.jar
-a----     25/06/2020  10:09 a. m.         183484 dreisoft.tresos.oilparser.jar
-a----     25/06/2020  10:09 a. m.       15842637 dreisoft.tresos.sysdimporter.jar
-a----     25/06/2020  10:09 a. m.         298269 dreisoft.tresos.tdbupgradev1v2.jar
-a----     25/06/2020  10:09 a. m.       33723980 dreisoft.tresos.tresosdb.api.jar
-a----     25/06/2020  10:09 a. m.          27076 dreisoft.tresos.tresosdbimporter.jar
-a----     25/06/2020  10:09 a. m.         134233 dreisoft.tresos.workflow.api.jar
-a----     30/01/2025  04:41 p. m.        5307122 eb.tresos.doc.studio.developers.documentation.en.jar
-a----     30/01/2025  04:41 p. m.           1001 eb.tresos.doc.studio.developers.documentation.jar
-a----     30/01/2025  04:41 p. m.       13325591 eb.tresos.doc.studio.documentation.en.jar
-a----     30/01/2025  04:41 p. m.            965 eb.tresos.doc.studio.documentation.jar
-a----     22/08/2024  10:31 a. m.          29240 freescale.tresos.flexray.jar
-a----     25/06/2020  10:09 a. m.        2442625 guava-20.0.jar
-a----     25/06/2020  10:09 a. m.          29148 javax.annotation_1.2.0.v201602091430.jar
-a----     25/06/2020  10:09 a. m.          55399 javax.el_2.2.0.v201303151357.jar
-a----     25/06/2020  10:09 a. m.          16996 javax.inject_1.0.0.v20091030.jar
-a----     25/06/2020  10:09 a. m.         111144 javax.servlet.jsp_2.2.0.v201112011158.jar
-a----     25/06/2020  10:09 a. m.         105237 javax.servlet_3.1.0.v201410161800.jar
-a----     25/06/2020  10:09 a. m.         252201 javax.xml_1.3.4.v201005080400.jar
-a----     25/06/2020  10:09 a. m.         356012 org.apache.batik.css_1.7.0.v201011041433.jar
-a----     25/06/2020  10:09 a. m.         212351 org.apache.batik.util.gui_1.7.0.v200903091627.jar
-a----     25/06/2020  10:09 a. m.         158140 org.apache.batik.util_1.7.0.v201011041433.jar
-a----     25/06/2020  10:09 a. m.         253506 org.apache.commons.jxpath.studio.jar
-a----     25/06/2020  10:09 a. m.         315491 org.apache.commons.jxpath_1.3.0.v200911051830.jar
-a----     25/06/2020  10:09 a. m.        2435771 org.apache.jasper.glassfish_2.2.2.v201501141630.jar
-a----     25/06/2020  10:09 a. m.         908681 org.apache.lucene.analysis_3.5.0.v20120725-1805.jar
-a----     25/06/2020  10:09 a. m.        1550172 org.apache.lucene.core_3.5.0.v20120725-1805.jar
-a----     25/06/2020  10:09 a. m.         108529 org.eclipse.ant.core_3.4.100.v20160505-0642.jar
-a----     25/06/2020  10:09 a. m.          66969 org.eclipse.compare.core_3.6.0.v20160418-1534.jar
-a----     25/06/2020  10:09 a. m.         799554 org.eclipse.compare_3.7.0.v20161024-1724.jar
-a----     25/06/2020  10:09 a. m.         115077 org.eclipse.core.commands_3.8.0.v20160316-1921.jar
-a----     25/06/2020  10:09 a. m.         101190 org.eclipse.core.contenttype_3.5.100.v20160418-1621.jar
-a----     25/06/2020  10:09 a. m.          80155 org.eclipse.core.databinding.beans_1.3.100.v20160509-1025.jar
-a----     25/06/2020  10:09 a. m.         354911 org.eclipse.core.databinding.observable_1.6.0.v20160511-1747.jar
-a----     25/06/2020  10:09 a. m.         196421 org.eclipse.core.databinding.property_1.6.0.v20160427-0852.jar
-a----     25/06/2020  10:09 a. m.         204409 org.eclipse.core.databinding_1.6.0.v20160412-0910.jar
-a----     25/06/2020  10:09 a. m.          91504 org.eclipse.core.expressions_3.5.100.v20160418-1621.jar
-a----     25/06/2020  10:09 a. m.         122203 org.eclipse.core.filebuffers_3.6.0.v20160503-1849.jar
-a----     25/06/2020  10:09 a. m.          10538 org.eclipse.core.filesystem.linux.x86_64_1.2.200.v20140124-1940.jar
-a----     25/06/2020  10:09 a. m.          31937 org.eclipse.core.filesystem.win32.x86_64_1.4.0.v20140124-1940.jar
-a----     25/06/2020  10:09 a. m.          66579 org.eclipse.core.filesystem_1.6.1.v20161113-2349.jar
-a----     25/06/2020  10:09 a. m.         111093 org.eclipse.core.jobs_3.8.0.v20160509-0411.jar
-a----     25/06/2020  10:09 a. m.          39432 org.eclipse.core.net.linux.x86_64_1.2.0.v20160323-1650.jar
-a----     25/06/2020  10:09 a. m.          29884 org.eclipse.core.net.win32.x86_64_1.1.0.v20160323-1650.jar
-a----     25/06/2020  10:09 a. m.          74341 org.eclipse.core.net_1.3.0.v20160418-1534.jar
-a----     25/06/2020  10:09 a. m.         882701 org.eclipse.core.resources_3.11.1.v20161107-2032.jar
-a----     25/06/2020  10:09 a. m.          75728 org.eclipse.core.runtime_3.12.0.v20160606-1342.jar
-a----     25/06/2020  10:09 a. m.          36017 org.eclipse.core.variables_3.3.0.v20160419-1720.jar
-a----     25/06/2020  10:09 a. m.         369550 org.eclipse.debug.core_3.10.100.v20160419-1720.jar
-a----     25/06/2020  10:09 a. m.        3111927 org.eclipse.debug.ui_3.11.202.v20161114-0338.jar
-a----     25/06/2020  10:09 a. m.          26000 org.eclipse.e4.core.commands_0.11.100.v20160506-0804.jar
-a----     25/06/2020  10:09 a. m.          48129 org.eclipse.e4.core.contexts_1.5.0.v20160504-0909.jar
-a----     25/06/2020  10:09 a. m.          11576 org.eclipse.e4.core.di.annotations_1.5.0.v20151127-1241.jar
-a----     25/06/2020  10:09 a. m.          27795 org.eclipse.e4.core.di.extensions_0.14.0.v20160211-1614.jar
-a----     25/06/2020  10:09 a. m.          54696 org.eclipse.e4.core.di_1.6.1.v20160712-0927.jar
-a----     25/06/2020  10:09 a. m.          54479 org.eclipse.e4.core.services_2.0.100.v20160509-1032.jar
-a----     25/06/2020  10:09 a. m.          50089 org.eclipse.e4.emf.xpath_0.1.200.v20160506-0804.jar
-a----     25/06/2020  10:09 a. m.          50737 org.eclipse.e4.ui.bindings_0.11.100.v20160509-1025.jar
-a----     25/06/2020  10:09 a. m.         215924 org.eclipse.e4.ui.css.core_0.12.1.v20161114-0210.jar
-a----     25/06/2020  10:09 a. m.          27497 org.eclipse.e4.ui.css.swt.theme_0.10.100.v20160523-0836.jar
-a----     25/06/2020  10:09 a. m.         259445 org.eclipse.e4.ui.css.swt_0.12.100.v20160517-1505.jar
-a----     25/06/2020  10:09 a. m.          16800 org.eclipse.e4.ui.di_1.1.100.v20160506-0759.jar
-a----     25/06/2020  10:09 a. m.         385199 org.eclipse.e4.ui.model.workbench_1.2.0.v20160229-1459.jar
-a----     25/06/2020  10:09 a. m.          28151 org.eclipse.e4.ui.services_1.2.100.v20160506-0759.jar
-a----     25/06/2020  10:09 a. m.          10605 org.eclipse.e4.ui.swt.gtk_1.0.100.v20160301-1001.jar
-a----     25/06/2020  10:09 a. m.          15378 org.eclipse.e4.ui.widgets_1.1.100.v20160506-0759.jar
-a----     25/06/2020  10:09 a. m.         152398 org.eclipse.e4.ui.workbench.addons.swt_1.2.100.v20160831-1151.jar
-a----     25/06/2020  10:09 a. m.         299608 org.eclipse.e4.ui.workbench.renderers.swt_0.14.0.v20160525-0940.jar
-a----     25/06/2020  10:09 a. m.         191811 org.eclipse.e4.ui.workbench.swt_0.14.1.v20160829-0832.jar
-a----     25/06/2020  10:09 a. m.          10954 org.eclipse.e4.ui.workbench3_0.13.100.v20160506-0759.jar
-a----     25/06/2020  10:09 a. m.         249245 org.eclipse.e4.ui.workbench_1.4.0.v20160517-1624.jar
-a----     25/06/2020  10:09 a. m.         289125 org.eclipse.emf.codegen_2.11.0.v20160526-0356.jar
-a----     25/06/2020  10:09 a. m.         357670 org.eclipse.emf.common_2.12.0.v20160420-0247.jar
-a----     25/06/2020  10:09 a. m.          87096 org.eclipse.emf.ecore.change_2.11.0.v20160420-0247.jar
-a----     25/06/2020  10:09 a. m.         230424 org.eclipse.emf.ecore.xmi_2.12.0.v20160420-0247.jar
-a----     25/06/2020  10:09 a. m.        1190945 org.eclipse.emf.ecore_2.12.0.v20160420-0247.jar
-a----     25/06/2020  10:09 a. m.          87568 org.eclipse.equinox.app_1.3.400.v20150715-1528.jar
-a----     25/06/2020  10:09 a. m.          49755 org.eclipse.equinox.bidi_1.0.0.v20160307-1318.jar
-a----     25/06/2020  10:09 a. m.         120435 org.eclipse.equinox.common_3.8.0.v20160509-1230.jar
-a----     25/06/2020  10:09 a. m.         196894 org.eclipse.equinox.ds_1.4.400.v20160226-2036.jar
-a----     25/06/2020  10:09 a. m.          34366 org.eclipse.equinox.event_1.3.200.v20160324-1850.jar
-a----     25/06/2020  10:09 a. m.          64629 org.eclipse.equinox.frameworkadmin.equinox_1.0.700.v20160102-2223.jar
-a----     25/06/2020  10:09 a. m.          37428 org.eclipse.equinox.frameworkadmin_2.0.300.v20160504-1450.jar
-a----     25/06/2020  10:09 a. m.          29927 org.eclipse.equinox.http.jetty_3.3.0.v20160324-1850.jar
-a----     25/06/2020  10:09 a. m.          46284 org.eclipse.equinox.http.registry_1.1.400.v20150715-1528.jar
-a----     25/06/2020  10:09 a. m.         185781 org.eclipse.equinox.http.servlet_1.3.1.v20160808-1329.jar
-a----     25/06/2020  10:09 a. m.          11992 org.eclipse.equinox.jsp.jasper.registry_1.0.300.v20130327-1442.jar
-a----     25/06/2020  10:09 a. m.          27958 org.eclipse.equinox.jsp.jasper_1.0.500.v20150119-1358.jar
-a----     25/06/2020  10:09 a. m.          51766 org.eclipse.equinox.launcher_1.3.201.v20161025-1711.jar
-a----     25/06/2020  10:09 a. m.         141186 org.eclipse.equinox.p2.artifact.repository_1.1.500.v20160419-0834.jar
-a----     25/06/2020  10:09 a. m.          73322 org.eclipse.equinox.p2.core_2.4.100.v20160419-0834.jar
-a----     25/06/2020  10:09 a. m.          54805 org.eclipse.equinox.p2.director.app_1.0.500.v20160419-0834.jar
-a----     25/06/2020  10:09 a. m.         104577 org.eclipse.equinox.p2.director_2.3.300.v20160504-1450.jar
-a----     25/06/2020  10:09 a. m.         207690 org.eclipse.equinox.p2.engine_2.4.100.v20160419-0834.jar
-a----     25/06/2020  10:09 a. m.          25987 org.eclipse.equinox.p2.garbagecollector_1.0.300.v20160504-1450.jar
-a----     25/06/2020  10:09 a. m.          72608 org.eclipse.equinox.p2.jarprocessor_1.0.500.v20160504-1450.jar
-a----     25/06/2020  10:09 a. m.         122479 org.eclipse.equinox.p2.metadata.repository_1.2.300.v20160419-0834.jar
-a----     25/06/2020  10:09 a. m.         343607 org.eclipse.equinox.p2.metadata_2.3.100.v20160427-2220.jar
-a----     25/06/2020  10:09 a. m.         233445 org.eclipse.equinox.p2.publisher.eclipse_1.2.100.v20160504-1450.jar
-a----     25/06/2020  10:09 a. m.          96264 org.eclipse.equinox.p2.publisher_1.4.100.v20160504-1450.jar
-a----     25/06/2020  10:09 a. m.         245107 org.eclipse.equinox.p2.repository.tools_2.1.300.v20160421-0324.jar
-a----     25/06/2020  10:09 a. m.         134293 org.eclipse.equinox.p2.repository_2.3.200.v20160421-0324.jar
-a----     25/06/2020  10:09 a. m.         128908 org.eclipse.equinox.p2.touchpoint.eclipse_2.1.400.v20160419-0834.jar
-a----     25/06/2020  10:09 a. m.          96069 org.eclipse.equinox.p2.updatesite_1.0.600.v20160504-1450.jar
-a----     25/06/2020  10:09 a. m.         133114 org.eclipse.equinox.preferences_3.6.1.v20160815-1406.jar
-a----     25/06/2020  10:09 a. m.         186860 org.eclipse.equinox.registry_3.6.100.v20160223-2218.jar
-a----     25/06/2020  10:09 a. m.         185694 org.eclipse.equinox.security.ui_1.1.300.v20150803-1225.jar
-a----     25/06/2020  10:09 a. m.          35190 org.eclipse.equinox.security.win32.x86_64_1.0.100.v20130327-1442.jar
-a----     25/06/2020  10:09 a. m.         109600 org.eclipse.equinox.security_1.2.200.v20150715-1528.jar
-a----     25/06/2020  10:09 a. m.          26379 org.eclipse.equinox.simpleconfigurator.manipulator_2.0.200.v20160504-1450.jar
-a----     25/06/2020  10:09 a. m.          44424 org.eclipse.equinox.simpleconfigurator_1.1.200.v20160504-1450.jar
-a----     25/06/2020  10:09 a. m.          77626 org.eclipse.equinox.util_1.0.500.v20130404-1337.jar
-a----     25/06/2020  10:09 a. m.         429486 org.eclipse.help.base_4.1.1.v20161124-1400.jar
-a----     25/06/2020  10:09 a. m.         508193 org.eclipse.help.ui_4.0.200.v20160510-0758.jar
-a----     25/06/2020  10:09 a. m.         637639 org.eclipse.help.webapp_3.8.0.v20160504-0839.jar
-a----     25/06/2020  10:09 a. m.         269916 org.eclipse.help_3.7.0.v20160602-1307.jar
-a----     25/06/2020  10:09 a. m.         169161 org.eclipse.jdt.compiler.apt_1.2.100.v20160418-1457.jar
-a----     25/06/2020  10:09 a. m.          69155 org.eclipse.jdt.compiler.tool_1.1.100.v20160418-1457.jar
-a----     25/06/2020  10:09 a. m.        5826018 org.eclipse.jdt.core_3.12.2.v20161117-1814.jar
-a----     25/06/2020  10:09 a. m.         343515 org.eclipse.jdt.launching_3.8.101.v20161111-2014.jar
-a----     25/06/2020  10:09 a. m.         159462 org.eclipse.jetty.http_9.3.9.v20160517.jar
-a----     25/06/2020  10:09 a. m.         119392 org.eclipse.jetty.io_9.3.9.v20160517.jar
-a----     25/06/2020  10:09 a. m.         105193 org.eclipse.jetty.security_9.3.9.v20160517.jar
-a----     25/06/2020  10:09 a. m.         512378 org.eclipse.jetty.server_9.3.9.v20160517.jar
-a----     25/06/2020  10:09 a. m.         126755 org.eclipse.jetty.servlet_9.3.9.v20160517.jar
-a----     25/06/2020  10:09 a. m.         458691 org.eclipse.jetty.util_9.3.9.v20160517.jar
-a----     25/06/2020  10:09 a. m.         290885 org.eclipse.jface.databinding_1.8.1.v20161026-1531.jar
-a----     25/06/2020  10:09 a. m.        1070533 org.eclipse.jface.text_3.11.2.v20161113-1700.jar
-a----     25/06/2020  10:09 a. m.        1086977 org.eclipse.jface_3.12.1.v20160923-1528.jar
-a----     25/06/2020  10:09 a. m.          42230 org.eclipse.jsch.core_1.3.0.v20160422-1917.jar
-a----     25/06/2020  10:09 a. m.         104621 org.eclipse.jsch.ui_1.3.0.v20160323-1650.jar
-a----     25/06/2020  10:09 a. m.         345037 org.eclipse.ltk.core.refactoring_3.7.0.v20160419-0705.jar
-a----     25/06/2020  10:09 a. m.         503766 org.eclipse.ltk.ui.refactoring_3.8.0.v20160518-1817.jar
-a----     25/06/2020  10:09 a. m.          28717 org.eclipse.nebula.widgets.pshelf_1.1.0.201609231530.jar
-a----     25/06/2020  10:09 a. m.          34486 org.eclipse.ocl.common_1.4.100.v20160613-1351.jar
-a----     25/06/2020  10:09 a. m.         244042 org.eclipse.osgi.compatibility.state_1.0.200.v20160504-1419.jar
-a----     25/06/2020  10:09 a. m.         111152 org.eclipse.osgi.services_3.5.100.v20160504-1419.jar
-a----     25/06/2020  10:09 a. m.        1383928 org.eclipse.osgi_3.11.2.v20161107-1947.jar
-a----     25/06/2020  10:09 a. m.        1304527 org.eclipse.pde.core_3.11.1.v20161115-1951.jar
-a----     25/06/2020  10:09 a. m.         169036 org.eclipse.pde.runtime_3.5.0.v20160418-1724.jar
-a----     25/06/2020  10:09 a. m.        8810009 org.eclipse.platform.doc.user_4.6.1.v20160727-2009.jar
-a----     25/06/2020  10:09 a. m.         510112 org.eclipse.search_3.11.1.v20161113-1700.jar
-a----     25/06/2020  10:09 a. m.        2767389 org.eclipse.swt.gtk.linux.x86_64_3.105.2.v20161122-0613.jar
-a----     25/06/2020  10:09 a. m.        2872411 org.eclipse.swt.win32.win32.x86_64_3.105.2.v20161122-0613.jar
-a----     25/06/2020  10:09 a. m.          19649 org.eclipse.swt_3.105.2.v20161122-0613.jar
-a----     25/06/2020  10:09 a. m.         426162 org.eclipse.team.core_3.8.0.v20160418-1534.jar
-a----     25/06/2020  10:09 a. m.         614115 org.eclipse.team.cvs.core_3.4.0.v20160418-1534.jar
-a----     25/06/2020  10:09 a. m.          30941 org.eclipse.team.cvs.ssh2_3.3.0.v20160418-1534.jar
-a----     25/06/2020  10:09 a. m.        1790551 org.eclipse.team.cvs.ui_3.4.0.v20160518-1906.jar
-a----     25/06/2020  10:09 a. m.        1536964 org.eclipse.team.ui_3.8.0.v20160518-1906.jar
-a----     25/06/2020  10:09 a. m.         269227 org.eclipse.text_3.6.0.v20160503-1849.jar
-a----     25/06/2020  10:09 a. m.         213276 org.eclipse.ui.console_3.6.201.v20161107-0337.jar
-a----     25/06/2020  10:09 a. m.         612214 org.eclipse.ui.editors_3.10.1.v20161106-1856.jar
-a----     25/06/2020  10:09 a. m.         348108 org.eclipse.ui.forms_3.7.0.v20160518-1929.jar
-a----     25/06/2020  10:09 a. m.          95438 org.eclipse.ui.ide.application_1.1.101.v20160829-0827.jar
-a----     25/06/2020  10:09 a. m.        2384816 org.eclipse.ui.ide_3.12.2.v20161115-1450.jar
-a----     25/06/2020  10:09 a. m.         328326 org.eclipse.ui.intro_3.5.2.v20161116-1147.jar
-a----     25/06/2020  10:09 a. m.         162342 org.eclipse.ui.navigator.resources_3.5.101.v20161006-0640.jar
-a----     25/06/2020  10:09 a. m.         437132 org.eclipse.ui.navigator_3.6.101.v20161006-1120.jar
-a----     25/06/2020  10:09 a. m.          51165 org.eclipse.ui.net_1.3.0.v20160426-1633.jar
-a----     25/06/2020  10:09 a. m.          71747 org.eclipse.ui.trace_1.0.400.v20160509-1055.jar
-a----     25/06/2020  10:09 a. m.         110526 org.eclipse.ui.views.properties.tabbed_3.7.0.v20160310-0903.jar
-a----     25/06/2020  10:09 a. m.         110524 org.eclipse.ui.views_3.8.101.v20160816-1954.jar
-a----     25/06/2020  10:09 a. m.          25969 org.eclipse.ui.win32_3.3.0.v20160505-1310.jar
-a----     25/06/2020  10:09 a. m.         667595 org.eclipse.ui.workbench.texteditor_3.10.1.v20160818-1626.jar
-a----     25/06/2020  10:09 a. m.        4040836 org.eclipse.ui.workbench_3.108.2.v20161025-2029.jar
-a----     25/06/2020  10:09 a. m.         396072 org.eclipse.ui_3.108.1.v20160929-1045.jar
-a----     25/06/2020  10:09 a. m.          90345 org.eclipse.uml2.common_2.1.0.v20160822-0739.jar
-a----     25/06/2020  10:09 a. m.          18871 org.eclipse.uml2.types_2.0.0.v20160822-0739.jar
-a----     25/06/2020  10:09 a. m.         102634 org.eclipse.update.configurator_3.3.400.v20160506-0750.jar
-a----     25/06/2020  10:09 a. m.         362968 org.sat4j.core_2.3.5.v201308161310.jar
-a----     25/06/2020  10:09 a. m.         241956 org.sat4j.pb_2.3.5.v201404071733.jar
-a----     25/06/2020  10:09 a. m.        3280108 org.tigris.subversion.clientadapter.javahl.win64_1.7.8.jar
-a----     25/06/2020  10:09 a. m.         167688 org.tigris.subversion.clientadapter.javahl_1.7.8.1.jar
-a----     25/06/2020  10:09 a. m.          83885 org.tigris.subversion.clientadapter_1.8.3.jar
-a----     25/06/2020  10:09 a. m.         328109 org.tigris.subversion.subclipse.core_1.8.16.jar
-a----     25/06/2020  10:09 a. m.        2342932 org.tigris.subversion.subclipse.doc_1.3.0.jar
-a----     25/06/2020  10:09 a. m.        2054352 org.tigris.subversion.subclipse.ui_1.8.18.jar
-a----     25/06/2020  10:09 a. m.         109753 org.tukaani.xz_1.3.0.v201308270617.jar
-a----     25/06/2020  10:09 a. m.          38584 org.w3c.css.sac_1.3.1.v200903091627.jar
-a----     25/06/2020  10:09 a. m.          18205 org.w3c.dom.events_3.0.0.draft20060413_v201105210656.jar
-a----     25/06/2020  10:09 a. m.          20106 org.w3c.dom.smil_1.0.1.v200903091627.jar
-a----     25/06/2020  10:09 a. m.          97382 org.w3c.dom.svg_1.1.0.v201011041433.jar

 

PS C:\NXP\SW32G_RTD_4.4_4.0.2_HF03\eclipse\plugins> Get-ChildItem -Depth 0


    Directory: C:\NXP\SW32G_RTD_4.4_4.0.2_HF03\eclipse\plugins


Mode                 LastWriteTime         Length Name
----                 -------------         ------ ----
d-----     12/12/2025  04:47 p. m.                Adc_TS_T40D11M40I2R0
d-----     12/12/2025  04:48 p. m.                BaseNXP_TS_T40D11M40I2R0
d-----     12/12/2025  04:48 p. m.                CanIf_TS_T40D11M40I2R0
d-----     12/12/2025  04:48 p. m.                Can_TS_T40D11M40I2R0
d-----     12/12/2025  04:48 p. m.                Crc_TS_T40D11M40I2R0
d-----     12/12/2025  04:48 p. m.                CryIf_TS_T40D11M40I2R0
d-----     12/12/2025  04:48 p. m.                Crypto_TS_T40D11M40I2R0
d-----     12/12/2025  04:48 p. m.                Csm_TS_T40D11M40I2R0
d-----     12/12/2025  04:48 p. m.                Dem_TS_T40D11M40I2R0
d-----     12/12/2025  04:48 p. m.                Det_TS_T40D11M40I2R0
d-----     12/12/2025  04:48 p. m.                Dio_TS_T40D11M40I2R0
d-----     12/12/2025  04:48 p. m.                EcuC_TS_T40D11M40I2R0
d-----     12/12/2025  04:48 p. m.                EcuM_TS_T40D11M40I2R0
d-----     12/12/2025  04:48 p. m.                Eep_TS_T40D11M40I2R0
d-----     12/12/2025  04:48 p. m.                EthIf_TS_T40D11M40I2R0
d-----     12/12/2025  04:48 p. m.                EthSwt_TS_T40D11M40I2R0
d-----     12/12/2025  04:48 p. m.                EthTrcv_TS_T40D11M40I2R0
d-----     15/12/2025  03:08 p. m.                Eth_43_PFE_TS_T40D11M12I0R0
d-----     12/12/2025  04:49 p. m.                Eth_TS_T40D11M40I2R0
d-----     12/12/2025  04:49 p. m.                Fee_TS_T40D11M40I2R0
d-----     12/12/2025  04:49 p. m.                Fls_TS_T40D11M40I2R0
d-----     12/12/2025  04:49 p. m.                FrIf_TS_T40D11M40I2R0
d-----     12/12/2025  04:49 p. m.                Fr_TS_T40D11M40I2R0
d-----     12/12/2025  04:49 p. m.                Gpt_TS_T40D11M40I2R0
d-----     12/12/2025  04:49 p. m.                I2c_TS_T40D11M40I2R0
d-----     12/12/2025  04:49 p. m.                Icu_TS_T40D11M40I2R0
d-----     12/12/2025  04:49 p. m.                LinIf_TS_T40D11M40I2R0
d-----     12/12/2025  04:50 p. m.                Lin_TS_T40D11M40I2R0
d-----     15/12/2025  03:08 p. m.                Mcl_TS_T40D11M40I2R0
d-----     12/12/2025  04:50 p. m.                Mcu_TS_T40D11M40I2R0
d-----     12/12/2025  04:50 p. m.                MemIf_TS_T40D11M40I2R0
d-----     12/12/2025  04:50 p. m.                Ocotp_TS_T40D11M40I2R0
d-----     12/12/2025  04:50 p. m.                Ocu_TS_T40D11M40I2R0
d-----     12/12/2025  04:50 p. m.                Os_TS_T40D11M40I2R0
d-----     12/12/2025  04:50 p. m.                Pcie_TS_T40D11M40I2R0
d-----     12/12/2025  04:50 p. m.                Platform_TS_T40D11M40I2R0
d-----     12/12/2025  04:50 p. m.                Pmic_TS_T40D11M40I2R0
d-----     12/12/2025  04:50 p. m.                Port_TS_T40D11M40I2R0
d-----     12/12/2025  04:50 p. m.                Pwm_TS_T40D11M40I2R0
d-----     12/12/2025  04:50 p. m.                Qdec_TS_T40D11M40I2R0
d-----     12/12/2025  04:50 p. m.                Resource_TS_T40D11M40I2R0
d-----     12/12/2025  04:50 p. m.                Rm_TS_T40D11M40I2R0
d-----     12/12/2025  04:50 p. m.                Rte_TS_T40D11M40I2R0
d-----     12/12/2025  04:50 p. m.                Serdes_TS_T40D11M40I2R0
d-----     12/12/2025  04:50 p. m.                Spi_TS_T40D11M40I2R0
d-----     12/12/2025  04:50 p. m.                Thermal_TS_T40D11M40I2R0
d-----     12/12/2025  04:50 p. m.                Uart_TS_T40D11M40I2R0
d-----     12/12/2025  04:50 p. m.                WdgIf_TS_T40D11M40I2R0
d-----     12/12/2025  04:51 p. m.                Wdg_43_VR5510_TS_T40D11M40I2R0
d-----     12/12/2025  04:51 p. m.                Wdg_TS_T40D11M40I2R0
-a----     22/08/2024  10:06 a. m.           2746 com.freescale.tools.tresos.xpath.jar
-a----     22/08/2024  10:23 a. m.           1757 com.nxp.tools.tresos.xpath.sqrt.jar
-a----     22/08/2024  10:31 a. m.          29240 freescale.tresos.flexray.jar

 

Then you can compare if there is any relevant difference in our plugin installation.

If you do not find any important difference, I would recommend trying reinstalling EB Tresos, if you have not already.

 

Please let me know if you find any information that might help me narrow down the problem.

0 Kudos
Reply

3,048 Views
Yang_C
Contributor IV

Hi alejandro_e,

Following your suggestion, I did the comparison, here is the result:

The output for C:\EB\tresos27\plugins, there're loads of differences.

As for the output for C:\NXP\SW32G_RTD_4.4_4.0.2_HF03\eclipse\plugins,  they are completely the same.

I will try reinstall the EB tresos on my end. Any updates I will let you know.

Thank you very much.

BR,

Yang

0 Kudos
Reply

2,962 Views
alejandro_e
NXP TechSupport
NXP TechSupport

Hello @Yang_C,

Were you able solve the problem after reinstalling EB Tresos Studio or were you able to get more information related to the issue?

 

Thanks 

0 Kudos
Reply

2,945 Views
Yang_C
Contributor IV

Hi alejandro_e,

Sorry for the late response. 

Unfortunately, I reinstalled EB tresos but the problem still persists. The issue is weird, I have decided to move on using Eth_43_PFE_TS_T40D11M14I0R0 for PFE configration. 

Thank you for your support anyway.

BR,

Yang

 

0 Kudos
Reply

2,939 Views
alejandro_e
NXP TechSupport
NXP TechSupport

Hello @Yang_C,

I am glad you were able to find a workaround for your problem. It is quite weird as you mentioned and I am sorry for not being of much help.

If in the future you encounter any other problem do not hesitate in creating a new post.

 

Best regards 

0 Kudos
Reply