Dual RISC processor in MSC8156

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Dual RISC processor in MSC8156

Jump to solution
3,968 Views
lpeng
Contributor I

Hi all,

The MSC8156 Block Diagram in document "MSC8156 Product Brief" show that MAPLE-B has a Dual RISC Engine, but the block Diagram in document "MSC8156 Data Sheet" show that there is no Dual RISC Engine in MAPLE-B and there are Dual RISC Processors in QUICC Engine Subsystem.

I want to ask whether both of their have Dual RISC processor. Thanks.

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
2,625 Views
starcoreDSP
Contributor II

Based on the 8156 RM, both MAPLE-B and QUICC Engine have Dual RISC Engine.  

 

In 8156 PB, on page 11, it says  

The QUICC Engine subsystem includes dual RISC processors and 48-Kbyte multi-master RAM
to handle the Ethernet and SPI interfaces, thus off loading the tasks from the cores. The three
communication controllers support

View solution in original post

0 Kudos
Reply
2 Replies
2,626 Views
starcoreDSP
Contributor II

Based on the 8156 RM, both MAPLE-B and QUICC Engine have Dual RISC Engine.  

 

In 8156 PB, on page 11, it says  

The QUICC Engine subsystem includes dual RISC processors and 48-Kbyte multi-master RAM
to handle the Ethernet and SPI interfaces, thus off loading the tasks from the cores. The three
communication controllers support

0 Kudos
Reply
2,625 Views
lpeng
Contributor I

Ok, Thank you. 

 

0 Kudos
Reply