Dual RISC processor in MSC8156

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Dual RISC processor in MSC8156

跳至解决方案
3,961 次查看
lpeng
Contributor I

Hi all,

The MSC8156 Block Diagram in document "MSC8156 Product Brief" show that MAPLE-B has a Dual RISC Engine, but the block Diagram in document "MSC8156 Data Sheet" show that there is no Dual RISC Engine in MAPLE-B and there are Dual RISC Processors in QUICC Engine Subsystem.

I want to ask whether both of their have Dual RISC processor. Thanks.

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
2,618 次查看
starcoreDSP
Contributor II

Based on the 8156 RM, both MAPLE-B and QUICC Engine have Dual RISC Engine.  

 

In 8156 PB, on page 11, it says  

The QUICC Engine subsystem includes dual RISC processors and 48-Kbyte multi-master RAM
to handle the Ethernet and SPI interfaces, thus off loading the tasks from the cores. The three
communication controllers support

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,619 次查看
starcoreDSP
Contributor II

Based on the 8156 RM, both MAPLE-B and QUICC Engine have Dual RISC Engine.  

 

In 8156 PB, on page 11, it says  

The QUICC Engine subsystem includes dual RISC processors and 48-Kbyte multi-master RAM
to handle the Ethernet and SPI interfaces, thus off loading the tasks from the cores. The three
communication controllers support

0 项奖励
回复
2,618 次查看
lpeng
Contributor I

Ok, Thank you. 

 

0 项奖励
回复