Does SJA1105S supports vlan forwarding

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does SJA1105S supports vlan forwarding

882件の閲覧回数
ramesh_mali
Contributor II

Hello,

I am working on the SJA1105S ethernet switch.

I have configuration parameter vlan forwarding type as:

1) NOT_SENT: message with the specific VLAN Id shall not be sent at this port.

2) SENT_TAGGED: message with the specific VLAN Id shall be sent with its VLAN Id at this port

3) SENT_TAGGED: message with the specific VLAN Id shall sent untagged

I am not able to find out which register setting i have to do so that particular switch port will work as per configured vlan forwarding type.

Regards

Ramesh

0 件の賞賛
返信
1 返信

816件の閲覧回数
bpe
NXP Employee
NXP Employee

VLAN-related settings are controlled in VLAN Lookup table, described
in Section 5.2.2. of  SJA1105P/Q/R/S Software User Manual (UM11040). Egress
tagging is controlled by TAG_PORT field, ports allowed to send out
frames with a given VLAN are specified as a mask in VMEMB_PORT.

Hope this helps,

Platon

0 件の賞賛
返信