Data encryption and protecting from hacking for security on PN7150

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Data encryption and protecting from hacking for security on PN7150

ソリューションへジャンプ
1,753件の閲覧回数
andy_kim
Contributor IV

Hello,

Let me ask about the amount of the security level of PN7150.

Application of our product is sharing network credentials between devices.

so security is most important factor.

 

We will use peer to peer mode of PN7150 for the application.

I wonder if PN7150 have a function of Data Encryption when communication with other device through NFC RF field and can protect data from hacking.

 

Best regards,

Andy

0 件の賞賛
返信
1 解決策
1,736件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @andy_kim ,

 

Do you want to implement a solution such as https://www.nxp.com/design/designs/layerscape-ls1012a-smart-home-gateway-reference-design:SMART-HOME... ?

Actually such kind of functionalities are usually handled on the host controller side, and we recommend using with a secure element  to achieve higher security . Please kindly refer to https://www.nxp.com/products/security-and-authentication/authentication/edgelock-se050-plug-trust-se... for more details.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,737件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @andy_kim ,

 

Do you want to implement a solution such as https://www.nxp.com/design/designs/layerscape-ls1012a-smart-home-gateway-reference-design:SMART-HOME... ?

Actually such kind of functionalities are usually handled on the host controller side, and we recommend using with a secure element  to achieve higher security . Please kindly refer to https://www.nxp.com/products/security-and-authentication/authentication/edgelock-se050-plug-trust-se... for more details.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

 

0 件の賞賛
返信