Control of outputs of MC33882 output switch

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Control of outputs of MC33882 output switch

跳至解决方案
1,673 次查看
ondrej_brejla
Contributor I

Hi,

I´m planning on using the MC33882 for realisation of digital outputs on a project I´m working on. I'm going to use the SPI interface to control the outputs. It's not really clear to me what should I do with the remaining input pins (IN0...IN7 and IN0&IN1 … IN4&IN5). Is it better to connect them to GND or just leave them with their internal pull down? Also should the unused outputs be left unconnected ?

Best regards,

Ondrej Brejla

0 项奖励
回复
1 解答
1,616 次查看
guoweisun
NXP TechSupport
NXP TechSupport

Hi,

For IN you can connect them to GND,for outputs you can floating.

Thanks!

在原帖中查看解决方案

1 回复
1,617 次查看
guoweisun
NXP TechSupport
NXP TechSupport

Hi,

For IN you can connect them to GND,for outputs you can floating.

Thanks!