Can't access PCIe in s32v234 boards

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can't access PCIe in s32v234 boards

1,210件の閲覧回数
steven_leon
Contributor I

Tried to access the PCIe device on two s32v234 boards, unsuccessfully.

In U-Boot, pci commands, such as enum, get a "pci_bus_to_hose() failed" message.

With Lauterbach, tried accessing the PCIe section in its built-in register mechanism, and also accessing directly the address stated in the Reference Manual (0x72000000 - 0x72ffffff). In both cases I get a debug port time out error.

Does U-Boot not clock the PCIe bus on this board? Is it disabled through some other means?

Thanks.

0 件の賞賛
返信
2 返答(返信)

1,171件の閲覧回数
steven_leon
Contributor I

Hi Tushar,

That's correct, same topic.

Yes, it can be closed here.

Thanks.

0 件の賞賛
返信

1,176件の閲覧回数
nxf92355
NXP Employee
NXP Employee

Hi Stevon 

I think you have raised new ticket in nxp as "PCIe inaccessible in s32v234 boards" . this both ticket are same. can we close here and continue in nxp support ? 

Regards ,

Tushar

0 件の賞賛
返信