Can i pullup the IRQ output of the SC16IS750IBS to 5V ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can i pullup the IRQ output of the SC16IS750IBS to 5V ?

ソリューションへジャンプ
650件の閲覧回数
HarryD
Contributor I

THe title basicialy states my question.

In the datasheet there is only a maximum current and no maximum voltage.

0 件の賞賛
返信
1 解決策
639件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Harry,

No, the maximum absolute ratings for the /IRQ pin is VDD + 0.3V which is below 5V.

BRs, Tomas

元の投稿で解決策を見る

2 返答(返信)
637件の閲覧回数
HarryD
Contributor I

Thank you !

0 件の賞賛
返信
640件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Harry,

No, the maximum absolute ratings for the /IRQ pin is VDD + 0.3V which is below 5V.

BRs, Tomas