Can i pullup the IRQ output of the SC16IS750IBS to 5V ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can i pullup the IRQ output of the SC16IS750IBS to 5V ?

Jump to solution
641 Views
HarryD
Contributor I

THe title basicialy states my question.

In the datasheet there is only a maximum current and no maximum voltage.

0 Kudos
Reply
1 Solution
630 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Harry,

No, the maximum absolute ratings for the /IRQ pin is VDD + 0.3V which is below 5V.

BRs, Tomas

View solution in original post

2 Replies
628 Views
HarryD
Contributor I

Thank you !

0 Kudos
Reply
631 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Harry,

No, the maximum absolute ratings for the /IRQ pin is VDD + 0.3V which is below 5V.

BRs, Tomas