CAN Implementation in LPC2129

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CAN Implementation in LPC2129

3,374件の閲覧回数
akhileshverneka
Contributor II

Sir I am working on Implementation of CAN protocol for LPC2129 board.Sir,When I  select CAN RX and CANTX  pin then the CAN TX line is Idle.But when I select only CAN TX then I get correct output.Please help me solve this issue.

タグ(3)
0 件の賞賛
返信
2 返答(返信)

3,325件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Akhilesh,

Regarding your question, as you know that the CAN bus is a bus architecture, each CAN node can transmit it's packet to CAN bus, so the arbitration is required, the lower number CAN ID has the higher priority. For arbitration, when the CAN node transmits ID via CAN_TX pin, the CAN_RX of the same CAN module has to receive the ID at the same time so that it can detect if the other CAN node is transmitting. So it does not make sense  if you do not connect CAN transceiver and just test the CAN_TX, after you connect CAN transceiver, the CAN_RX can receive the packet the CAN node transmits and the arbitration can be done.

I attach the CAN transceiver schematics, hope it can help you

BR

XiangJun Rong

3,325件の閲覧回数
akhileshverneka
Contributor II

Thank you 

0 件の賞賛
返信