Booting Problem with imx21ads in linux.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Booting Problem with imx21ads in linux.

2,400 Views
srisindhu
Contributor I
Hi,
I have Imx21Ads board with me. The host environment is  fedora 5.
I am able to successfully flash bootloader using imx21_download and able to flash ramdisk and kernel through blob prompt.
After flashing kernel, when i give "boot" command in blob prompt,
it hangs after displaying  the following message
 
Uncompressing Linux.............................................. done, bootin.
 
Can anyone help me what the problem is.
Here Iam attaching screenshot of the blob.
 
thanks in advance,
srisindhu
0 Kudos
Reply
2 Replies

1,432 Views
arthas
Contributor I
What version is about your blob bootloader ?
Maybe your extern IO not init ?
 
 
you can add debug to arch/arm/kernel/head.S
and see debug info!
 
 
0 Kudos
Reply

1,432 Views
Rame
Contributor I
Hi,

I am also facing the same problem. Anyone suggest what could be the problem.

Regards
Ramesh
0 Kudos
Reply