AFT27S010NT1 maximum current

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

AFT27S010NT1 maximum current

3,197 次查看
alleniub
Contributor I

I don't see the maximum ID current or Output power in the AFT27S010NT1 datasheet, is there a related limit ?

 

 

@AFT27S010NT1

0 项奖励
回复
7 回复数

3,186 次查看
diazmarin09
NXP TechSupport
NXP TechSupport

Hello,

I hope all is great with you.

Please review the typical characteristics below:

diazmarin09_0-1662413268468.png

 

diazmarin09_1-1662413273064.png

 

You may find further information about all its frequency range at AFT27S010N datasheet.

I hope this information helps.

Regards,

David

0 项奖励
回复

3,183 次查看
alleniub
Contributor I

I would like to ask if there is a maximum Continuous Drain Current?, in my simulation the ID current is around 2A. Is this acceptable?

0 项奖励
回复

3,174 次查看
diazmarin09
NXP TechSupport
NXP TechSupport

Hello,

I am pleased to contact you again.

I am afraid that such information is not characterized.

I have requested further information. If I receive a response, I will inform you as soon as possible.

Regards,

David

0 项奖励
回复

3,168 次查看
alleniub
Contributor I

2022-09-09 010031.jpg2022-09-09 011742.jpg

I mean is there a maximum drain current like the above table, I just want to make sure my simulation drain current 2A is ok . 

0 项奖励
回复

3,166 次查看
diazmarin09
NXP TechSupport
NXP TechSupport

Hello,

Please accept my apologies for the misunderstanding.

The AFT27S010N is optimized for Class AB operation. Idq is typically set at 90mA.  Depending on output power level desired.

Class A operation would require an Idq of around 1000mA.

I hope this information helps.

Regards,

David

0 项奖励
回复

3,150 次查看
alleniub
Contributor I

In my simulation, with the transistor operating at class E, IDS(ON) is about 2A.

From your answer I'm not sure if the transistor can withstand 2A (AC),

thanks

0 项奖励
回复

3,126 次查看
diazmarin09
NXP TechSupport
NXP TechSupport

Hello,

I am pleased to contact you again. I hope all is great with you.

You are correct, based on the statement above, the device might not withstand such operational conditions.

I hope this information helps.

Regards,

David

0 项奖励
回复