AFT05MS003N Questions

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

AFT05MS003N Questions

ソリューションへジャンプ
1,751件の閲覧回数
languer
Contributor II

Seems this is the only channel for product support anymore. So I will post my product support questions here.

Are there s-parameters for the AFT05MS003N which go down to, say 50MHz?

Can the AFT05MS003N be biased at +5V?

Any insight on noise figure (typical) at 100MHz-150MHz?

ラベル(1)
  • RF

タグ(1)
0 件の賞賛
返信
1 解決策
1,467件の閲覧回数
languer
Contributor II

Product support answered this as follows:

AFT05MS003N_PDK can be used to predict operational performance at +5V drain voltage. Freescale/NXP MET LDMOS Model is an empirical large signal nonlinear model and is capable of performing small-signal, large-signal, harmonic-balance, noise and transient simulations.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,468件の閲覧回数
languer
Contributor II

Product support answered this as follows:

AFT05MS003N_PDK can be used to predict operational performance at +5V drain voltage. Freescale/NXP MET LDMOS Model is an empirical large signal nonlinear model and is capable of performing small-signal, large-signal, harmonic-balance, noise and transient simulations.
0 件の賞賛
返信