ADC doubts

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ADC doubts

1,263件の閲覧回数
snehalpatil
Contributor II

Can anyone plz explain me this function

adc16_status_t ADC16_DRV_ConfigConvChn(uint32_t instance, uint32_t chnGroup, const adc16-configPtr);

what parameter instance and chngroup means?

How to initialize and assign multiple channels ( differential input) for ADC conversion in continuous conversion mode?

If I want to use 3 channels as ADC inputs is it possible to initialize 2 channels as differential input and 1 as single ended input? If its possible how it should be done?

0 件の賞賛
返信
3 返答(返信)

1,145件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Hello Snehal

Could you please supply the part number of your target MCU? And are you using SDK or any other tool which supplies the function ADC16_DRV_ConfigConvChn()?

And if you are developing with CodeWarrior or KDS, you may use Processor Expert to configure ADC easily, including assign multiple channels in continuous conversion mode.

Best Regards

Fiona Kuang

Technical Information & Commercial Support

0 件の賞賛
返信

1,145件の閲覧回数
snehalpatil
Contributor II

Hi,

We are using MK02FN128VFM10 part number. Yes we are using KDS. Actually I am new to it and don’t know how to use Processor Expert. It would be very good if you provide steps to use processor expert.

Regards,

Snehal.

0 件の賞賛
返信

1,145件の閲覧回数
snehalpatil
Contributor II

Request to reply as early as possible plz..........:smileysad:

0 件の賞賛
返信