已解决! 转到解答。
Dear Syf,
The following thread has examples for combined OSBDM/TBDML code for the JB16 in the 20p and 28p packages. Have alook at the files in the USBDM_Flash_Images folder for schematics and corresponding S19 files.
bye
now my computer can scan that a unkown usb hardware had been connected to it. but i can not update the driver.
and my scheme was designed for jb8. and now made some changes inorder to fit jb16 as follow:
1:use the 12mhz ossilitor
2:have a 10kohm pull up resistor on pin 12 of jb16.Connected the D+ and D- to gnd with 470kohm.
3:grounding the PTA0 , and made a power on reset circuit on pin 28 of jb16.
i don't kown why my computer can not update the driver for the found hardware.
Dear Syf,
The operation of the software is described in AP note 2399 available here:
AN2399 : In-Circuit Programming of FLASH Memory via the Universal Serial Bus for the MC68HC908JB16
Software available here:
AN2399SW : Software files for AN2399
The only real requirements are as you have indicated for a blank device:
pull-down on A.0
470K pull-downs on D+ & D-
100nF capacitor on reset
12MHz crystal (+ 2 capacitors) on EXTAL/XTAL
What is the 10K resistor for on pin 12 (PTE.3/D+?) This conflicts with the 470K resistor.
The required drivers are part of the software package above.
Could you check in the PC hardware manager if the device is identifying itself - check the VID/PID on the details page for the device.
bye
Dear Syf,
The following thread has examples for combined OSBDM/TBDML code for the JB16 in the 20p and 28p packages. Have alook at the files in the USBDM_Flash_Images folder for schematics and corresponding S19 files.
bye
Hi Pgo,
I have some problems on TBDML over JDWE 20 pin SOIC.I was able to enter ICP mode and download the TBDML code,but i see after programming ,my pc restarts the moment i unplug usb cable.Why is so?
Also i have used breadboard and intially after prgramming ,when i plug in ,idont see the usb detected ,but when i touch with my finger on any of the pins while plugging the cable,the usb detects and pc loads the driver.why is it so ,any grounding problems? Can you suggest any methods to resolve it?
Regards,
lazeee...
Dear Laz-e-Boy,
I haven't encountered any similar problems.
I would be very worried that there was some kind of short or similar on the power supply. Try isolating the BDM with an external hub and see if this has any effect on its operation.
I would check the wiring VERY carefully.
Are you sure you are not introducing external voltages to the USB power connections? Check the grounding between the USB cable and target power supply as well.
Sorry I can't be more helpfull. I have found the JB16 BDMs quite reliable.
bye
Hi pgo
i did some testing using below attached file and found the notebook detecting the usb and loads up the driver everytime i plug in,though i had success with this,i dont know why my notebook restarts after programming in ICP mode.H/Wwise a 10uf & 0.1uf capacitor isolates vdd and gnd,usb diff's are pull downs 470K's.
I havent connected the target micro circuit as i wanted to test the usb portion first.I will rewire and observe the behaviour today...
lazeeee...