MC13213

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC13213

1,608 Views
danielt3
Contributor I

Hi all!

 

I'm using a MC13213 system-on-chip from Freescale in my undergratuate final project in college. But the problem is that I don't any hardware to burn/debug the code in the uc inside MC13213 (MC9S08GT) . I would like to know if I can use OSBDM with this particular chip to burn/debug my code inside CodeWarrior? 

 

 

thanks in advance 

Tags (2)
0 Kudos
Reply
1 Reply

303 Views
pgo
Senior Contributor V

Dear Danielt3,

 

I don't have a MC13213 module to test but it would appear from the Spec sheet that it has the standard BDM interface available.  OSBDM is supported as a target for the MC9S08GT in Codewarrior so I would be surprised if it did not work with the MC1321.

 

bye

 

0 Kudos
Reply