USBDM Hardware Debugging in KDS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USBDM Hardware Debugging in KDS

15,119 Views
ebee
Contributor II

When I try to set up USBDM Hardware Debugging in KDS I am getting the message 'An error occurred. See error log for more details'. The initial error message is 'net/sourceforge/usbdm/constants/UsbdmSharedConstants$InterfaceType'.

I have attached the error log report,

0 Kudos
Reply
28 Replies

9,618 Views
ebee
Contributor II

Hi pgo,

I have downloaded and installed the new version 4.10.6.170 and I am still getting the same error messages.

I have also downloaded the release version of KDS and the same error message occurs when I try to use the USBDM debugger in this one too.

Regards

Ian

0 Kudos
Reply

9,618 Views
FredericoLuiz
Contributor II

Hi Ian,

can you debug now using USBDM hardware in KDS? I'd like to do so but until now I'm able.

If you get your problem solved, please let me know how did you make it.

Thanks.

Frederico

0 Kudos
Reply

9,620 Views
pgo
Senior Contributor V

Hi Ian,

This looks like it can't find one of the plugins - probably because it failed to load or was the wrong version.

Can I find check the following:

  • What version of USBDM is installed?
  • When exactly is this error occurring?  During the creation of the Debug Launch configuration?

Also please check the following:

  • Make sure there are not any bits left over from other versions of USBDM.  For example if your installed an earlier version that didn't have the KDS installation and and manually copied the plugin files into the ...\Freescale\KDS_1.0.1\eclipse\dropins directory it will be necessary to delete these.  Later installers don't have this problem.
  • Can you check the USBDM plugin versions installed in KDS.  This can be done by
    • Selecting : Help->About Kinetis Design Studio
    • Then Installation Details button
    • Select Plug-ins tab
    • Click on the Plug-in Id column header to sort the column.
    • The list should be similar to that shown below.

pastedImage_4.pngpastedImage_7.pngpastedImage_8.png

pastedImage_0.png

bye

0 Kudos
Reply

9,620 Views
ebee
Contributor II

I am running version 4.10.6.160 of the USBDM software. The error occurs when I try to create the Debug Launch configuration.

I did start off with an earlier version of USBDM that did not automatically detect the KDS installation so I used the configuration within the installer to install the plug ins into KDS1.0.1 etc. I have checked the contents of the dropins folder and all the files are date stamped 31/05/2014 which is the same as most of the files in my current pgo installation directory so it does not look as though anything has been left behind in here. I had an arm_devices.xml file left over from 4.10.6.140 in its own directory but that is the only file that I had modified. I have now deleted this file and the same error occurs.

For the plugins I have all the same file names as you on your list but the version numbers for everything is 4.10.6.201405311721 with the exception of USBDM Peripheral View which has the version number 1.0.0.201405311721.

I have had it working but recently for developing a multi processor system I have moved the USBDM device to a USB port on a hub rather than having it connected to my default debug port on my computer. The other device is debugging over J-Link. On the computer the USBDM device appears as a USB Composite device. On the hub the same device appears as a USBDM HCS08,HCS12,CFV1,ARM_SWD_BDM (I am debugging an ARM device over SWD). If I plug it into the computer USB port or the hub it still does not work within KDS.

If I connect the device to the PC USB port I can still use the ARM Programmer utility to program the micro controller, this does not work on the hub where it can not find a BDM device.

0 Kudos
Reply

9,620 Views
pgo
Senior Contributor V

Hi Ian,

I'm a bit unclear about your description above.  Does the plugin work with KDS if the BDM is plugged directly into the machine?

Anyway, I suspect there is a problem with loading one of the plugins (net.sourceforge.usbdm.constants).  This handles paths to USBDM amongst other things.

Could I get you do do the following:

  • Open the Error Log (Window->Show View->Error Log) You may need to search for it under Other.
  • Clear the log using the Big Red X
  • Restart KDS
  • Check for any messages relating to USBDM in the log.
  • Try your failing process
  • Re-check the error log to see if there are any errors (other than the one you quoted above).

Thanks

bye

0 Kudos
Reply

9,620 Views
ebee
Contributor II

Hi pgo,

Sorry about the confusion. The plug is is not working within KDS where ever I plug the BDM in.

I have followed the instructions that you gave. On restarting KDS there was not any messages relating to USBDM in the log. When I try to connect to the debugger two new errors occur -

Problems occurred when invoking code from plug-in: "org.eclipse.jface". in plug in org.eclise.jface.

An error occurred while automatically activating bundle net.sourceforge.usbdm.contstants (464) in plugin org.eclispe.osgi

I have attached the full (or as much as I can get) error reportserror2.pngerror1.png

0 Kudos
Reply

9,620 Views
pgo
Senior Contributor V

Hi Ian,

The second exception looks more hopeful for a clue.

It appears that one of the plugins is throwing an exception when loading.  Probably processing the USBDM paths but there isn't enough information to be sure.

I should have asked you to post the .metadata\.log file from the workspace you are using as this contains the entire log.

Would you please repeat clearing the log and triggering the exceptions?

Clearing the log first will reduce the "clutter" in the .log file.

I have installed USBDM 4.10.6.160 from sourceforge on another machine but it also appears to work OK with KDS.

Do you have any regular eclipse installations with USBDM installed.  If so, are there any problems with them?

One last thing to check:

  • Open the USBDM configuration form the menu (USBDM->Configuration) and check that all the pages look OK.

Thanks

0 Kudos
Reply

9,620 Views
ebee
Contributor II

Hi pgo,

I tried going diown the uninstall route and that has not resolved the problems.

I uninstalled the KDS installation. Checked for any files / folders left behind and removed these.

I uninstalled the USBDM installation. Checked for any files / folders left behind and removed these.

Reinstalled KDS using the full installation. Opened KDS and checked for any updates - nothing to get.

Reinstalled USBDM from USBDM_4_10_6_160_Win.msi.

I still get the same errors when I try to connect via the KDS. I do not know what else I can try now.

regards

Ian

0 Kudos
Reply

9,620 Views
pgo
Senior Contributor V

Hi Ian,

I'm sorry I've been unavailable for a little while.

The trace you posted indicates that the plugin is failing to load the the JNI (Java Native Interface) code  and the associated DLL usbdm.4.dll.

I can't reproduce this on the machines I tried but it may be due to OS related problem.

Could you post details about the Operating System you are using and I will try to do some more specific testing.

Thanks

0 Kudos
Reply

9,620 Views
RichC
Contributor I

Hi pgo

Sorry for adding a "me too" post, but I've hit this same plugin JNI issue on Windows 7 x64. It's been working reliably for weeks, but today it refuses to cooperate! I guess it's probably something changed on my machine in the time I haven't been using KDS, but even clean reinstalls of KDS/USBDM don't fix it for me.


If I launch the USBDM ARM programmer from the start menu, it will happily detect the device, so it really just seems to be the JNI part of the eclipse plug in which is failing.

Any pointers on how I can start tracking things down or tools which may help please - I'm running out of places to look :-)

Further background, in case it sparks any ideas:

It may be a coincidence, but I recently did an upgrade JetBrains WebStorm (v8 to v9).  I'd hope WebStorm and KDS wouldn't fight each other, but perhaps there is one global eclipse setting somewhere that I can't find - I tried checking the registry and env variables, but nothing obvious leapt out waving a big red flag.


In desperation I've now uninstalled WebStorm 9 entirely then reinstalled only KDS (1.1.1), USBDM (4.10.6.230)  and drivers (1.3.0 Win x64). But alas the error is still there when I go to the USBDM menu > Configure

Thanks,

Rich.

0 Kudos
Reply

9,620 Views
RichC
Contributor I

So, I've managed to get this working again, but without really understanding what has gone wrong with the plugin system. Documenting as best I can here in case it helps future visitors.

The underlying error, reported by Windows, is actually no entry point found in usbdm.4.dll on the path:  C:\Freescale\KDS_1.1.1\eclipse\configuration\org.eclipse.osgi\bundles\451\1\.cp\usbdm4.dll

At this point, there are only 3 dlls in the directory libgcc_s_dw2-1.dll, libstdc++-6.dll and usbdm.4.dll. I assume they are getting unpacked from net.sourceforge.usbdm.jni_4.10.6.201412010002.jar

However the dll sizes are smaller than the equivalent dlls in C:\Program Files (x86)\pgo\USBDM 4.10.6.230\ which is what I installed.

So, my work around was to copy the larger usbdm.4.dll over the top. This fixes the JNI issue when trying to open the USBDM > Configure menu. I can't guarantee it's the 'correct' workaround, but it's got me able to debug again :-)

0 Kudos
Reply

9,620 Views
pgo
Senior Contributor V

Hi Richard,

I'm glad you found a work-around.

I will check the two DLLs and see if I can reconcile the differences.

In general I have found the JNI stuff a bit fragile so I don't usually change anything unless there is a reason.  Because of this it is not surprising that the DLLs may be different builds i.e. updated in the main files but not in the plugin.

It is strange that the same plugin works with Codewarrior.

Can I check a few things:

  • Is your installation within the  Program Files (x86) directory?  The permissions applied by windows differ if installed there.  I usually install Eclipse-based tools to a "Apps" directory to avoid issues.
  • It may be worthwhile to run Eclipse with the "-initialize" option e.g. "C:\Apps\Freescale\KDS_2.0.0\eclipse\kinetis-design-studio.exe -initialize" to cause KDS to rescan the plugins. Don't do this if it's working!

bye

0 Kudos
Reply

9,618 Views
RichC
Contributor I

Thanks for -initialize suggestion. I won't run it now as I have a working system, but good to know for the future.

Yes, my usbdm installation is under the Program Files (x86).


Edit: You may have been asking about KDS? This is installed to c:\Freescale\KDS_1.1.1\...


I still don't understand how it worked for a few weeks before failing and which dll it was using during that time. Maybe KDS hiccuped and reinitialised, or windows update changed the behaviour of loading dlls or security settings. For future reference I should mention that I'm using Win 7 SP1 x64, patched with Jan 2015's updates.



0 Kudos
Reply

9,620 Views
JeffLynne
Contributor II

DLL mismatch is the issue!.

Situation is KDS2.0.0 and USBDM4.10.6.250! Initally I was also getting error trying to reach any menu concerning USBD.

I've checked the 'bundles' directory e.g. "Freescale\KDS_1.1.1\eclipse\configuration\org.eclipse.osgi\bundles\xxxx" - and the *.dll in plugin directory were

different size (usbdm4.dll was different version also, seen from properties)!!!!


I just copied all DLLs from the instalation directory in Program Files .... and voila! error disappeared, now all menus are accesible without error and debuging the target is also working.


0 Kudos
Reply

9,620 Views
RichC
Contributor I

Jeff,   Good to know that combination KDS 2.0.0 and  USBDM4.10.6.250 works. One of my many attempted installs yesterday was KDS2.0.0 + USBDM 10.6.230, but gdb server didn't launch for me so I settled for a combination that worked from me in the past (1.1.1 and 4.6.10.230).


Could I ask how you have configured the directory paths for the plugin? as I think that's probably what I had wrong in 2.0.0.

Thanks.

0 Kudos
Reply

9,619 Views
pgo
Senior Contributor V

Hi Richard & Jeff,

The DLLs are different of course but I still can't understand why this would result in problems.

The eclipse plugin doesn't use the extra entry points and (of course) it works on the machines I tried.

The same plugin is used with Codewarrior and has been reported to work on the same machine as KDS fails so I'm thoroughly confused.

Any way I will update the plugin to be consistent and also add the refresh options to the installation process in case that is contributing (V4.10.6.250a).

Could I ask one of you to try one more test to confirm that the DLL build is the problem?

  • Restore the original DLL and check if the problem re-surfaces?

Thanks

0 Kudos
Reply

9,618 Views
RichC
Contributor I

Extracted: usbdm.4.dll from net.sourceforge.usbdm.jni_4.10.6.210412010002.jar

it is 163,840 bytes, version 4.10.5.0 and copied it into my KDS 'bundles'


Yes, it stops working immediately. Here is the debug trace from an attached Visual Studio debugger:

The thread 'Win32 Thread' (0xfac) has exited with code 0 (0x0).

'kinetis-design-studio.exe': Loaded 'C:\Freescale\KDS_1.1.1\eclipse\configuration\org.eclipse.osgi\bundles\450\1\.cp\libgcc_s_dw2-1.dll', Binary was not built with debug information.

'kinetis-design-studio.exe': Loaded 'C:\Freescale\KDS_1.1.1\eclipse\configuration\org.eclipse.osgi\bundles\450\1\.cp\libstdc++-6.dll', Binary was not built with debug information.

'kinetis-design-studio.exe': Loaded 'C:\Freescale\KDS_1.1.1\eclipse\configuration\org.eclipse.osgi\bundles\450\1\.cp\usbdm.4.dll', Binary was not built with debug information.

First-chance exception at 0x77911d82 in kinetis-design-studio.exe: 0xC0000139: Entry Point Not Found.

'kinetis-design-studio.exe': Unloaded 'C:\Freescale\KDS_1.1.1\eclipse\configuration\org.eclipse.osgi\bundles\450\1\.cp\usbdm.4.dll'

The thread 'Win32 Thread' (0x508) has exited with code 0 (0x0).

And recopying in the 4.10.6.230 (164,864 bytes) makes it work again. (I have only been replacing that single DLL, Jeff seems to have replaced all 3 or 4 dlls)

Could it be that the smaller dll  depends on some other runtime lib which is not (or no longer) on our systems? Just a wild guess really!

0 Kudos
Reply

9,618 Views
pgo
Senior Contributor V

Hi Richard,

Thanks for the quick feedback!

I did use a dependency checker on the original and larger DLL and they both appear to have the same dependency tree below.

Anyway it must be some subtle problem (or at least too subtle for me!).  I have been caught before with the system picking up a DLL from somewhere else on my machine and hiding a problem like this so I suspect it is something like this.

Thanks again for taking the time to troubleshoot this.

I will upload an updated build tonight and I hope it will solve this.

bye

pastedImage_0.png

0 Kudos
Reply

9,618 Views
RichC
Contributor I

Hi pgo,

I'm in a position to test a fresh install of the eclipse plugin this week, is it USBDM_4_10_6_250a_Win.msi that includes your fixes to the JNI Dll version?

Thanks.

0 Kudos
Reply

9,618 Views
pgo
Senior Contributor V

Hi Richard,

Yes the 250a version installer runs eclipse/KDS with the "-initialize" option and also includes the "fixed" (I hope) plugins.

I would appreciate you testing this.

I will be getting a new computer in the near future and I will do some similar tests.

Thanks.

0 Kudos
Reply