TBDML support HCS08

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

TBDML support HCS08

8,461 次查看
nihke
Contributor I
TBDML support HCS08.
MC9S08RD16 test OK with CodeWarrior 5.0.
[admin note: a large attachment dating from 2007 has been removed. large attachments are no longer supported in the forums]
Message Edited by t.dowe on 2009-09-23 09:18 AM
0 项奖励
回复
7 回复数

1,817 次查看
nihke
Contributor I
I will go to have a look at the current vision,thanks.
then I will change it support on TBDML.
0 项奖励
回复

1,817 次查看
nihke
Contributor I
I have changed the bdm.c and usb.c.It is used on TBDML now.
0 项奖励
回复

1,817 次查看
Alban
Senior Contributor II
Hi again,

I think I now understand you adapted the code of the OSBDM08 for S08 to be supported via TBDML.
It is a very good news, thanks for the work.

Does it also support the S12 in the same time ?
Cheers,
Alban.
0 项奖励
回复

1,817 次查看
nihke
Contributor I
Hi,
sorry for HCS12.
0 项奖励
回复

1,817 次查看
nihke
Contributor I
Please change .ZIP to .rar,that will be OK.
0 项奖励
回复

1,817 次查看
Alban
Senior Contributor II
Hello,

This project is not based on the TBDML but is the OSBDM08.
I can advise you to look at other versions of the OSBDM08 in the OSBDM08 dedicated board.

The more current versions have some additional features that would simplify your life on top of also supporting the RS08 family
0 项奖励
回复

1,817 次查看
Alban
Senior Contributor II
Ni Hao,

TBDML and Open Source BDM are two different projects.
Open Source BDM is calles OSBDM08 and has its own forum group: OSBDM08: Open Source BDM for (R)S08

I cannot open your zip file. Can you please check if it is working for you ?
Xiexie,
Alban.
0 项奖励
回复