TBDML support HCS08

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TBDML support HCS08

9,901件の閲覧回数
nihke
Contributor I
TBDML support HCS08.
MC9S08RD16 test OK with CodeWarrior 5.0.
[admin note: a large attachment dating from 2007 has been removed. large attachments are no longer supported in the forums]
Message Edited by t.dowe on 2009-09-23 09:18 AM
0 件の賞賛
返信
7 返答(返信)

3,257件の閲覧回数
nihke
Contributor I
I will go to have a look at the current vision,thanks.
then I will change it support on TBDML.
0 件の賞賛
返信

3,257件の閲覧回数
nihke
Contributor I
I have changed the bdm.c and usb.c.It is used on TBDML now.
0 件の賞賛
返信

3,257件の閲覧回数
Alban
Senior Contributor II
Hi again,

I think I now understand you adapted the code of the OSBDM08 for S08 to be supported via TBDML.
It is a very good news, thanks for the work.

Does it also support the S12 in the same time ?
Cheers,
Alban.
0 件の賞賛
返信

3,257件の閲覧回数
nihke
Contributor I
Hi,
sorry for HCS12.
0 件の賞賛
返信

3,257件の閲覧回数
nihke
Contributor I
Please change .ZIP to .rar,that will be OK.
0 件の賞賛
返信

3,257件の閲覧回数
Alban
Senior Contributor II
Hello,

This project is not based on the TBDML but is the OSBDM08.
I can advise you to look at other versions of the OSBDM08 in the OSBDM08 dedicated board.

The more current versions have some additional features that would simplify your life on top of also supporting the RS08 family
0 件の賞賛
返信

3,257件の閲覧回数
Alban
Senior Contributor II
Ni Hao,

TBDML and Open Source BDM are two different projects.
Open Source BDM is calles OSBDM08 and has its own forum group: OSBDM08: Open Source BDM for (R)S08

I cannot open your zip file. Can you please check if it is working for you ?
Xiexie,
Alban.
0 件の賞賛
返信