Problem with "Can't connect. USBDM device is not open" error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem with "Can't connect. USBDM device is not open" error

576件の閲覧回数
gashtaan
Contributor I

I'm developing firmware for MC9S08GB60A MCU in CodeWarrior for MCU 11.1 using USBDM I bought on AliExpress. It's based on MC9S08JS16CWJ MCU. I updated it to the latest USBDM firmware. Everything works OK, I can compile and run/debug the firmware, but only once in during CodeWarrior session. Next time I try to download and run/debug the firmware I got "HC/RS/S12Z GDI Protocol Adapter : Can't connect. USBDM device is not open" error. If I close the CodeWarrior application and open it again, it works OK, but only once. Any idea what is wrong with it?

0 件の賞賛
返信
1 返信

237件の閲覧回数
gashtaan
Contributor I

Is no one experiencing the same behavior?

0 件の賞賛
返信