I meet a question when I program MC9S08PA4 through USBDM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

I meet a question when I program MC9S08PA4 through USBDM

1,438 次查看
wangbaode
Contributor IV

Hi,

I meet a question when I program MC9S08PA4.

I can detect the chip and erase the chip through USBDM.but the chip can't be programmed through USBDM.

USBDM问题.jpg

My USBDM firmware is 4.10.5.USBDM hardware is USBDM_SWD_SER_JS16CWJ_V2.0.

could you try it ?

标记 (1)
0 项奖励
回复
4 回复数

1,104 次查看
pgo
Senior Contributor V

Hi Wang,

The PA4 and PA2 are not supported by USDBM at the moment due to the limited amount of RAM available in combination with the new Flash technology.

I will have to re-write the drivers to do this.  I had a look at this last week end but it is quite difficult so I'm unsure when they will be supported.

bye

0 项奖励
回复

1,104 次查看
wangbaode
Contributor IV

Hi pgo,

Thanks for your answer. I just want to make sure the question.

Thanks for your work in usbdm again.

0 项奖励
回复

1,104 次查看
pgo
Senior Contributor V

Hi Wang,

USBDM_4_10_6_60.Win.msi, just uploaded to sourceforge, adds support for MC9S08PA4 and MC9S08PA2.

bye

0 项奖励
回复

1,104 次查看
wangbaode
Contributor IV

Hi pgo,

Thank you!

0 项奖励
回复