I have a patch to USBDM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I have a patch to USBDM

1,206件の閲覧回数
galadragos
Contributor III

I made a few changes in order to get USBDM to compile on my linux distribution (fedora)

 

First of let me say that I have imported the trunk folder of the project from github directly into eclipse.

 

Here are my contributions:

- new script "CreateBinDir" which is a modified version of the .deb creator and will create a directory in which you can find all the binaries of USBDM so you can copy it's content to "/" (drive root) ;

- patched makefile to include the linux directory for java, similar to windows include, so it can find java_md.h

- patched makefile to check for existence of tcl8.5/tcl.h and to signal it's presence there

- patched usbdmTcl.c to include either tcl.h or tcl8.5/tcl.h, based on above patch

 

Other things I have noticed:

- CaMeL case problems! Could not find some program headers because the directory and header filename was CaMeLcAsEd which work only on crapwin filesystems

 

Please try not to use camel case file and folder names as it will have disastrous effects on filesystems which are case sensitive.

 

I have attached the eclipse generated patch file.

Original Attachment has been moved to: usbdm_patch.txt.zip

タグ(2)
0 件の賞賛
返信
1 返信

855件の閲覧回数
galadragos
Contributor III

pgo, have you managed to get a look at the patch ?

0 件の賞賛
返信