Hi pgo, okay I'm not getting the microcontroller mc9s12hz256 add the list of supported devices could help me?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Hi pgo, okay I'm not getting the microcontroller mc9s12hz256 add the list of supported devices could help me?

902件の閲覧回数
jackbonys
Contributor I

Hi pgo, okay I'm not getting the microcontroller mc9s12hz256 add the list of supported devices could help me?

<device family="HCS12" name="MC9S12HZ256">

   <clock type="External" />

   <memory type="ram">

      <memoryRange  start="0x1000" end="0x3FFF" />

   </memory>

   <memory registerAddress="0x0110" type="eeprom" sectorSize="2" alignment="2">

      <memoryRange  start="0x0400" end="0x07FF" />

   </memory>

   <memory registerAddress="0x0100" type="flash" securityAddress="0xFF0F" sectorSize="256" alignment="2" >">

<securityEntryRef ref="HCS12-default-security" />

      <memoryRange start="0x4000" end="0x7FFF" />

       <memoryRange start="0x8000" end="0xBFFF" />

         <memoryRange start="0xC000" end="0xFFFF" />

</memory>

    <sdid value="0x1403" />

  <flashScripts>

            <tclScriptRef ref="HCS12-FTMRCK-flash-scripts" />

         </flashScripts>

         <flashProgramRef ref="HCS12-PMMC-FTMRCK-flash-program" />

     

to where I am going wrong?

0 件の賞賛
返信
1 返信

688件の閲覧回数
pgo
Senior Contributor V

Hi Thiago,

(This is a copy of a reply to a PM - Copy here for reference)

Try to following and see if it is any more successful.  Note I don't have a chip to test with.

bye

  <device family="HCS12" name="MC9S12HZ256">

        <clock type="External" />

        <memory type="ram">

            <memoryRange start="0x1000" end="0x3FFF" />

        </memory>

        <memory registerAddress="0x0110" type="eeprom" sectorSize="4" alignment="2">

            <memoryRange start="0x000400" end="0x0007FF" />

        </memory>

        <memory pageAddress="0x0030" registerAddress="0x0100" type="flash" securityAddress="0xFF00" sectorSize="1024" alignment="8">

            <securityEntryRef ref="HCS12-default-security" />

            <memoryRange start="0x4000" end="0x7FFF" /> <!-- Page 3E -->

            <memoryRange start="0x8000" end="0xBFFF" pages="256K"  pageEnd="0x3F" />

            <memoryRange start="0xC000" end="0xFFFF" /> <!-- Page 3F -->

        </memory>

        <sdid value="0x1402" />

        <sdid value="0x1403" />

        <flashProgramRef ref="HCS12-MMCV4-FTS_2-flash-program" />

   </device>

If this doesn't work please try running the debug version of the programmer (available in the USBDM installation directory) and then post the log files (available in %APPDATA%\usbdm).

The needed files are FlashProgrammer_HCS12.log, and usbdm.log.

I don;t have this chip to test so it's a bit painful to work out what is wrong.

Thanks

0 件の賞賛
返信