yes, its TBDML
I connect bdm and reset line by 3,4k ohm to 5V from USB.
effect is always the same after start TrueTimeSimulator$RealTimeDebuger:
http://www.musiq.pl/~majkel/HW.GIF"Unable to connect to the target CPU"
iam using latest CW4.5 ,
MC912DT128A and MC9S12DT256B both with 16MHz
I tested all connection and dont know what can be wrong??
which setting of J5 and J6 are reccomend??
is any method to test the TBDML if it works fine to exclude problem with it and concentrate on target bord and conection. a thing a shema of TBDML is ok and there wasnt any problem in programing it and install USB DLL.
Message Edited by Michail on
2007-05-14 04:38 PM