Failed to resume target process. Downloading binary to target...

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Failed to resume target process. Downloading binary to target...

ソリューションへジャンプ
2,544件の閲覧回数
Joel69003
Contributor IV

Hi all, and particularly PGO,

I'm experimenting issues with CodeWarrior and the USBDM with MKE02Z64M4 device. I have created a project and keep all default options. However, it is not possible to load and debug the application. I get the following error when launching the debugging:

error.PNG

In the console:

console.PNG

My USBDM is "USBDM_SWD_JS16CWJ". Software version is 4.10.6.200, drivers 1.3.0.

I am able to program the target with the ARM programmer provided with the USBDM (it works well) but it is not very convenient to debug the application...

Have you experimented this kind of issues ? Thanks for your help!

Regards,

Joel

0 件の賞賛
返信
1 解決策
1,992件の閲覧回数
pgo
Senior Contributor V

Hi Joel,

The current version adds these aliases so I would expect it to work now.

bye

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
1,992件の閲覧回数
pgo
Senior Contributor V

Hi Joel,

It is not setting the device correctly (Hence the _DEFAULT) in the flash programming log.

This probably means that I have not correctly set an alias for the device.  Codewarrior uses different names internally for devices and these are mapped to the usual names by an alias entry in the database.

I probably have missed the one for the device you are using.

I will check this.

bye

PS Confirmed missing entries.  This will be corrected in the next version or you can try manually adding the following lines to near the end of arm_devices.xml (after similar ones for KE02Z16M2):

  <device name="KE02Z16M4"     alias="MKE02Z16M4"    hidden="true"/>
  <device name="KE02Z32M4"     alias="MKE02Z32M4"    hidden="true"/>
  <device name="KE02Z64M4"     alias="MKE02Z64M4"    hidden="true"/>

bye

1,992件の閲覧回数
Joel69003
Contributor IV

Hello PGO,

Thanks for writing. I have added the 3 lines in the file "C:\Program Files (x86)\pgo\USBDM 4.10.6.200\DeviceData\arm_devices.xml" just below the three lines for KE02 M2 devices but it is not working :-( I have created a new project in a new workspace, and it is still written "DEVICE = '_DEFAULT'" in the console. Do I need to do something to force CodeWarrior taking care of the new configuration ?

Note: I have created a new project with a KE02 M2 device (well, I don't now the difference between the two except the maximum clock speed) and launched the debug of a very simple application with CodeWarrior and it is working. So issue is only for the M4 devices.

Thanks for your help,

Regards,

Joel

0 件の賞賛
返信
1,993件の閲覧回数
pgo
Senior Contributor V

Hi Joel,

The current version adds these aliases so I would expect it to work now.

bye

0 件の賞賛
返信
1,992件の閲覧回数
wangyongsheng
Contributor I

Hello PGO

I meet the same problems using the USBDM 4.10.6.250 to Debug the DSC MC56F8345 and MC56F84789 with Codewarrior 10.6.But the information in Console is different.Here is the details:

Executing Initialization File: E:\Codewarrior\84789_BDM/Project_Settings/Debugger/MC56F84789.tcl

radix x

cmdwin::eclipse::config hexprefix 0x

cmdwin::eclipse::config MemWidth 16

cmdwin::eclipse::config MemAccess 16

cmdwin::eclipse::config MemSwap off

Starting 3rd party flash programming...

DiMemoryDownload() - DI_DNLD_TERMINATE - Programming memory image...

===========================================================

Programming target

  Device = 'MC56F84585'

  Trim, F=0, NVA@0000, clock@0000

  Ram[0000...3FFF]

  Erase=EraseMass

  Security=intelligent

  Total bytes=35556

  doRamWrites=T

Erase Time = 3.48 s, Speed = 9.97 kBytes/s, rc = 0

DiMemoryDownload() - DI_DNLD_TERMINATE - Programming complete, rc = 7

    Thanks for your attention,

    Best Regards,

    yongsheng

0 件の賞賛
返信
1,992件の閲覧回数
Joel69003
Contributor IV

Hi PGO,

I have installed 4.10.6.210 and the issue is now corrected.

Thanks for your time.

Best Regards,

Joel

0 件の賞賛
返信