Hello PGO
I meet the same problems using the USBDM 4.10.6.250 to Debug the DSC MC56F8345 and MC56F84789 with Codewarrior 10.6.But the information in Console is different.Here is the details:
Executing Initialization File: E:\Codewarrior\84789_BDM/Project_Settings/Debugger/MC56F84789.tcl
radix x
cmdwin::eclipse::config hexprefix 0x
cmdwin::eclipse::config MemWidth 16
cmdwin::eclipse::config MemAccess 16
cmdwin::eclipse::config MemSwap off
Starting 3rd party flash programming...
DiMemoryDownload() - DI_DNLD_TERMINATE - Programming memory image...
===========================================================
Programming target
Device = 'MC56F84585'
Trim, F=0, NVA@0000, clock@0000
Ram[0000...3FFF]
Erase=EraseMass
Security=intelligent
Total bytes=35556
doRamWrites=T
Erase Time = 3.48 s, Speed = 9.97 kBytes/s, rc = 0
DiMemoryDownload() - DI_DNLD_TERMINATE - Programming complete, rc = 7
Thanks for your attention,
Best Regards,
yongsheng