Error Message

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error Message

3,964件の閲覧回数
admin
Specialist II
Hi,
Does anyone know what this error message mean?

Code:

Communication settings:
SETCOMM DRIVER PROTOCOL NOPERIODICAL
Error: Device list is empty!!!!
SETCOMM DRIVER PROTOCOL|NOPROTOCOL PERIODICAL|NOPERIODICAL "<path to the GDI driver DLL>"
SETCOMM COMPORT NONE|USB|LPT|ETHERNET|ETHERNETFIP "<com device name>"
SETCOMM IPADDRESS "<IP address>"
GDI:   DiGdiClose(TRUE)
Communication settings:
SETCOMM DRIVER PROTOCOL NOPERIODICAL
Loading Communication DLL
 ==> L:\CodeWarrior V6.1\prog\gdi\OSBDM_S08.dll
GDI:   DiGdiOpen()==> DI_OK
GDI:   DiGdiVersion()==> DI_ERR_NOTSUPPORTED
GDI:   DiGdiAddCallBack(8192)==> DI_OK
GDI:   DiGdiAddCallBack(16384)==> DI_OK
GDI:   DiCommGetAcceptableSettings()==> 5
GDI:   DiCommGetAcceptableSettings()==> 0
GDI:   DiCommGetAcceptableSettings()==> 5
Error: Device list is empty!!!!
SETCOMM DRIVER PROTOCOL|NOPROTOCOL PERIODICAL|NOPERIODICAL "<path to the GDI driver DLL>"
SETCOMM COMPORT NONE|USB|LPT|ETHERNET|ETHERNETFIP "<com device name>"
SETCOMM IPADDRESS "<IP address>"



 My BDM was working very consistantly well for a while until now, I just can not connect to the target QG8...



ラベル(2)
タグ(2)
0 件の賞賛
返信
2 返答(返信)

1,354件の閲覧回数
goldensea
Contributor I
BDM lost connection with PC.
connect USB cable again.
0 件の賞賛
返信

1,354件の閲覧回数
AndreCG
Contributor I

Hi

 

I'm having the same problem. It doesn't work any more, even if I disconect and conect again.

 

 

What's going on?

 

hugs 

 

André

 

0 件の賞賛
返信