Debugging problem with USB Multilink Universal

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Debugging problem with USB Multilink Universal

ソリューションへジャンプ
2,164件の閲覧回数
oakie_doke
Contributor III

Hi,

I'm working with CodeWarrior 10.6 and MCF51MM256 (Coldfire V1). I was working with USB BDM Multilink debug interface for few months and everything was ok. Now I'm using USB Multilink Universal and there is problem when I debug my project.

no source.bmp

I found that program crashes in __initialize_hardware() function while MCGC1 register is setting. I configure internal bus clock 24MHz. When I set lower value of clock everything is ok.

Problem is similar to:

What is the maximum frenqency of OSBDM ?

About s12ZVH clock configuration on CW10.6-PE

There is solution to use USB Multilink Universal but I use it now.

This is my configuration:

internal clock.bmp

Do you have any suggestion?

0 件の賞賛
返信
1 解決策
1,885件の閲覧回数
oakie_doke
Contributor III

Solved. Firmware update of USB Multilink Universal helped.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,886件の閲覧回数
oakie_doke
Contributor III

Solved. Firmware update of USB Multilink Universal helped.

0 件の賞賛
返信