Debugging problem with USB Multilink Universal

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Debugging problem with USB Multilink Universal

跳至解决方案
2,175 次查看
oakie_doke
Contributor III

Hi,

I'm working with CodeWarrior 10.6 and MCF51MM256 (Coldfire V1). I was working with USB BDM Multilink debug interface for few months and everything was ok. Now I'm using USB Multilink Universal and there is problem when I debug my project.

no source.bmp

I found that program crashes in __initialize_hardware() function while MCGC1 register is setting. I configure internal bus clock 24MHz. When I set lower value of clock everything is ok.

Problem is similar to:

What is the maximum frenqency of OSBDM ?

About s12ZVH clock configuration on CW10.6-PE

There is solution to use USB Multilink Universal but I use it now.

This is my configuration:

internal clock.bmp

Do you have any suggestion?

0 项奖励
回复
1 解答
1,896 次查看
oakie_doke
Contributor III

Solved. Firmware update of USB Multilink Universal helped.

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,897 次查看
oakie_doke
Contributor III

Solved. Firmware update of USB Multilink Universal helped.

0 项奖励
回复