Problem playing video using gplay

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem playing video using gplay

ソリューションへジャンプ
3,370件の閲覧回数
admin
Specialist II

Hi,

We are testing videos on the i.MX6DL AI board with L3.0.35_4.0.0, using the command “$gplay BD1280.mkv”.  One video can’t be played by gplay but it can be played using L3.10.17_1.0.0 BSP. Could you please provide suggestions about this issue? Does the VPU firmware have to be updated for L3.0.35_4.0.0/4.1.0?

Thanks for your help.

0 件の賞賛
1 解決策
3,007件の閲覧回数
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

元の投稿で解決策を見る

0 件の賞賛
2 返答(返信)
3,008件の閲覧回数
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 件の賞賛
3,007件の閲覧回数
stephencox
NXP Pro Support
NXP Pro Support

The mkv parser in 3.10.17 can be used to resolve the issue in 3.0.35_4.0.0.  Bring in the file “lib_mkv_parser_arm11_elinux*” from Kernel 3.10.17 and all should be good.

0 件の賞賛