Problem playing video using gplay

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem playing video using gplay

Jump to solution
3,416 Views
admin
Specialist II

Hi,

We are testing videos on the i.MX6DL AI board with L3.0.35_4.0.0, using the command “$gplay BD1280.mkv”.  One video can’t be played by gplay but it can be played using L3.10.17_1.0.0 BSP. Could you please provide suggestions about this issue? Does the VPU firmware have to be updated for L3.0.35_4.0.0/4.1.0?

Thanks for your help.

0 Kudos
1 Solution
3,053 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

View solution in original post

0 Kudos
2 Replies
3,054 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 Kudos
3,053 Views
stephencox
NXP Pro Support
NXP Pro Support

The mkv parser in 3.10.17 can be used to resolve the issue in 3.0.35_4.0.0.  Bring in the file “lib_mkv_parser_arm11_elinux*” from Kernel 3.10.17 and all should be good.

0 Kudos