NXPトレーニングコンテンツ

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NXP Training Content

ディスカッション

ソート順:
Design, Software and Services Accelerating Firmware Development of Kinetis MCUs by using the New Peripheral Drives, Stacks and Middleware of Kinetis SDK Hands-On Workshop: MQX™ RTOS and Kinetis Software Development Kit (SDK) Integration   Smart Industry Hands-On Workshop: Introduction to the Development of Embedded Systems with Asymmetric Multicore Approach Networking Applications with Yocto Project™ Operation Presenting the New QorIQ LS1 MPUs for IoT, M2M
記事全体を表示
Design, Software and Services Insight and Innovation Smart Industry
記事全体を表示
This session will address how S12 MagniV mixed-signal MCUs can help customers design more compact and cost-effective electronic control units. The S12 MagniV devices are built on proven S12 technology, enabling software and tool compatibility across the entire portfolio. With the right blend of digital programmability and high-precision analog, plus a portfolio of scalable memory options, the S12 MagniV portfolio streamlines automotive design. Presented at DwF MCU Solutions - Zhengzhou - 31 March 2015 Session ID: APF-ACC-T0982
記事全体を表示
Ethercat, Profinet, PROFIBUS, CAN, RS232, etc. are extensively used in communications networks in factories, buildings, transport infrastructures and monitoring/control equipment in our cities. Technologies such as EtherCAT, PROFINET and EtherNet/IP are testament to this. In this session, we will explore how QorIQ LS1 processor families can help equipment manufacturers span this landscape using a QUICC Engine (QE) controller for UART/Ethernet-based protocol implementation, an Enhanced Triple Speed Ethernet Controller (eTSEC) for intelligent Ethernet classification and 2-port switching, and an eight-port gigabit Ethernet switch for wire-rate switching. Further we will look on how QorIQ LS1 family meet the emerging Internet of Things (IoT) requirements as also as the Broadband Home router and NAS market. Presented by Gino Gatto Presented at DwF Istanbul and Ankara- May 12 and 14, 2015 Session ID: EUF-SNT-T1468
記事全体を表示
Automotive and Connected Car Design, Software and Services
記事全体を表示
Learn how an image flows through an i.MX 6 series or i.MX5x applications processor from the sensor, through the image processing unit (IPU), all the way to the display. Learn to set up and control the image path, as well as where the BSP and Uboot must be touched to effect changes. This session will include an instructor-led demonstration based on i.MX 6 series applications processors and homework. Presented by: Oliver Brown Presented at: FTF 2014 Session ID: FTF-CON-F0119
記事全体を表示
Presented at DwF RF Solutions - Wuhan
記事全体を表示
Introduce sensor hub and fusion solutions, and update the latest sensor product and roadmap.  Presented by Eric Wu Presented at DwF Taipei - May 7, 2015 Session ID: APF-INS-T1457
記事全体を表示
Smart Home and Buildings Wi-Fi Module from Freescale and QualComm Smart Networks K22FSH Development
記事全体を表示
Presented by James Huang Presented at DwF Hsinchu
記事全体を表示
This hands-on session will detail how to build portable and diagnostic devices using the Kinetis ARM® Cortex®-M0 and Cortex-M4 products from Freescale. Special attention will be paid to the integration of sensors and Bluetooth® low energy. Presented by: aleguzman Presented at: FTF 2014 Session ID: FTF-HCR-F0197
記事全体を表示
Are you ready for kernel 3.10.53? Learn how to boot with the device tree, understand bindings and syntax today. Presented by Massimo Bonazzi Presented at DwF Istanbul and Ankara - May 12 and 14, 2015 Session ID: EUF-DES-T1465
記事全体を表示
Advanced driver assist systems (ADAS) and autonomous driving (AD) require a combination of high-performance processing and functional safety. There is currently no single SoC capable of meeting AD performance requirements with the intrinsic safety capabilities required for expected regulatory requirements. To facilitate development and testing of AD sensor inputs, vehicle control algorithms, and functional safety fault detection and response mechanisms, Freescale has developed prototype ECU hardware based on a high-performance ‘Number Cruncher’ and an ISO 26262 ‘Safety Controller’, which we call the Blue Box. This session covers the Blue Box hardware and software features, and intended usage.
記事全体を表示
Freescale is the best positioned silicon maker for the Internet of Tomorrow. This session is all about how Freescale sees the mechanics of the IOT. Attend this session and see what runs under the hood! Presented by Massimo Bonazzi Presented at DwF Istanbul and Ankara - May 12 and 14, 2015 Session ID: EUF-IND-T1463
記事全体を表示
Smart Home and Buildings Hands-On Workshop: IoT Wi-Fi Module Development Kit - Quick Start Smart Networks
記事全体を表示
Presented at DwF RF Solutions - Wuhan Presented by Song Di
記事全体を表示
This session will explain how to migrate between the QorIQ T2081 and T1040 communications processor families by achieving hardware and software compatibility. The session will also discuss hardware, software and board-level considerations that exist while migrating between these processors and designing a common board for these processors. Presented by You Peng Presented at DwF Digital Networking - Nanjing - 21 May 2015 Session ID: APF-SNT-T1360
記事全体を表示
ARM Processors i.MX 2014 Archives Kinetis Power Architecture Processors QorIQ Analog and Power Management RF Sensors 2014 Archives Wireless Connectivity 2014 Archives Medical and Healthcare 2014 Archives Additional Courses Material
記事全体を表示