NXP Model-Based Design Tools Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXP Model-Based Design Tools Knowledge Base

Discussions

Sort by:
This page summarizes all Model-Based Design Toolbox tutorials and articles related to DSC MCUs Product Family.
View full article
This page summarizes all Model-Based Design Toolbox videos related to DSC MCUs Product Family.
View full article
General Tip of the day Tip of the day  Model Reference Model referencing in i.MX RT Toolbox  Peripherals FLEXCAN How to set i.MX RT FlexCAN receive message buffer Mask for range of IDs ?   LPI2C How to use LPI2C in transfer mode in i.MX RT  LPUART Questions about i.MX RT LPUART driver  Apps
View full article
General Installer and Setup  External mode External mode example wouldn't compile after update  Others MPC57xx MBD Toolbox not appears in Simulink Library Browser  Peripherals Apps Motor Control BMS Request for HSD/LSD/MSDI Communication Examples for MPC5775B BMS and VCU Reference Design 
View full article
General Tip of the day Tip of the day  Licensing MBDT license missing error  Toolbox functionality Registers, Linkers not displaying options  Profiler/Execution S32k144 Simulation Time and Profiler  Peripherals How to put MCU into sleep? Apps Motor Control
View full article
This page summarizes all Model-Based Design Toolbox videos related to HCP Product Family. Deploying Radar Applications to NXP´s S32R41 Processor Using Simulink® Link to the recording here This webinar shows how to use Radar Toolbox, Simulink ®  , and Embedded Coder ®  to generate C code for radar signal processing algorithms for range and speed estimation and deploy them to NXP ® ´s S32R41 high-performance processor for high-resolution radar. Based on MathWorks´ radar example models, we use Embedded Coder to generate optimized C code and run it in Processor-in-the-Loop (PIL) mode on the S32R41 processor. The code generation workflow will feature the use of NXP´s Model-Based Design Toolbox (MBDT), which provides an integrated development environment and toolchain for configuring and generating all the necessary software to execute complex applications on NXP MCUs and processors.
View full article
This page summarizes all Model-Based Design Toolbox videos related to S32K3 Product Family.  NXP MBDT - S32K3 Updates In this video, we discuss the Model-Based Design paradigm and how to take advantage of the MathWorks ecosystem to generate C code automatically for the NXP S32K3xx. We start our discussion with details about MBDT Concept, Development flow, and Advantages. Then we compare the NXP's MBDT for S32K1 vs MBDT for S32K3 where we introduce the usage of an "external configuration" tool to handle the MCU Clocks, Pins, and Components configuration particular the NXP S32 Configuration Tools and EB tresos Studio. We then explain how the new paradigm matches a "true" Model-Based Design Approach and helps the development engineers. Finally, we discuss the Toolbox for S32K3, what NXP products integrate, and what applications look like. Deploying AUTOSAR ™  and Non-AUTOSAR Software Components on NXP S32K3 with MathWorks ®  Tools Link to the recording here AUTOSAR ™  Classic is the proven standard for traditional automotive applications such as powertrain, chassis, body and interior electronics and more. More frequently, OEMs and suppliers would prefer to reuse the tested and proven legacy (non- AUTOSAR) ECU software in next-generation AUTOSAR ECUs. In this webinar, NXP and MathWorks will show how to use NXP Model-Based Design Toolbox (MBDT) together with MathWorks ®  Simulink ®  and Embedded Coder ®  to develop and deploy MCAL configured (non-AUTOSAR) applications on NXP S32K3 microcontrollers for general purpose. Furthermore, we will illustrate how to convert tested non-AUTOSAR application components to AUTOSAR and then verify and deploy MCAL configured AUTOSAR compliant production code on an S32K3 MCU. Deploying a Deep Learning-Based State-of-Charge (SoC) Estimation Algorithm to NXP S32K3 Microcontrollers Link to the recording here Battery management systems (BMS) ensure safe and efficient operation of battery packs in electric vehicles, grid power storage systems, and other battery-driven equipment. One major task of the BMS is estimating state of charge (SoC). Traditional methods for SoC estimation require accurate battery models that are difficult to characterize. An alternative to this is to create data driven models of the cell using AI methods such as neural networks. This webinar shows how to use Deep Learning Toolbox, Simulink, and Embedded Coder to generate C code for AI algorithms for battery SoC estimation and deploy them to an NXP S32K3 microcontroller. Based on previous work done by McMaster University on Deep Learning workflows for battery state estimation, we use Embedded Coder to generate optimized C code from a neural network imported from TensorFlow and run it in processor-in-the-loop mode on an NXP S32K3 microcontroller. The code generation workflow will feature the use of the NXP Model-Based Design Toolbox, which provides an integrated development environment and toolchain for configuring and generating all the necessary software to execute complex applications on NXP MCUs.  A Model-Based Design (MBDT) Environment for Motor Control Algorithm Development Link to the recording here  This webinar, co-hosted with MathWorks, shows how to design and develop Motor Control algorithms with Simulink ® , using the Embedded Coder and Model-Based Design Toolbox for S32K3xx. We will introduce the scalable S32K3 MCU family and present its specific motor control modules. We will show how to access and configure the MCU peripherals making the Simulink model hardware aware, and ready to generate, build and deploy the application on the hardware. We will focus on Field Oriented Control (FOC) algorithm and implement a sensorless control of a permanent magnet synchronous motor (PMSM). The FreeMASTER application will be used to control and monitor the algorithm running on the S32K344. NXP MBDT for S32K3 provides an integrated development environment and toolchain for configuring and generating all the necessary software to execute complex applications on NXP MCUs directly from Simulink ® .   Speed-Up BMS Application Development with NXP's High-Voltage Battery Management System Reference Design and Model-Based Design Toolbox (MBDT) Link to the recording here  This webinar shows how to design and develop Battery Management Systems, with NXP's High-Voltage BMS Reference Design and Model-Based Design Toolbox for S32K3xx, with Simulink® and Embedded Coder. During this webinar, we will introduce the ASIL D High Voltage Battery Management System Reference Resign that comprises a Battery Management Unit (BMU), Cell Monitoring Units (CMU), and a Battery Junction Box (BJB). NXP's HV-BMS Reference Design is a robust and scalable solution including hardware designs, production-ready software drivers, and safety libraries, as well as extensive ISO 26262 Functional Safety documentation. The design significantly reduces the development effort and enables an improved time to market with the latest chipset innovations. Speed Up Electrification Solutions Using NXP Tools Link to the recording here  This video provides an overview of the NXP Software and Tools solutions, designed to help customers to speed up application development with design, simulation, implementation, deployment, testing, and validation. During this session, you will learn about all the steps required to build complete solutions like battery management systems with NXP in-house solutions and NXP Model-Based Design Toolbox with simulation and code generation.
View full article
This page summarizes all Model-Based Design Toolbox tutorials and articles related to HCP Product Family.   S32G2 Hybrid Electrical Vehicle (HEV) demo on S32G2 
View full article
This page summarizes all Model-Based Design Toolbox tutorials and articles related to S32K3xx Product Family.
View full article
This page summarizes all Model-Based Design Toolbox topics related to the HCP Product Family. Model-Based Design Toolbox for HCP - Release Notes: Rev 1.3.0 - NXP Model-Based Design Toolbox for High-Performance Computing Platform (HCP) - version 1.3.0 RFP  Rev 1.2.0 - NXP Model-Based Design Toolbox for High-Performance Computing Platform (HCP) - version 1.2.0 RFP  Rev 1.1.0 - NXP Model-Based Design Toolbox for High-Performance Computing Platform (HCP) - version 1.1.0 RFP  Rev 1.0.0 - Model-Based Design Toolbox for High-Performance Computing Platform (HCP) - version 1.0.0 EAR 
View full article
This page summarizes all Model-Based Design Toolbox topics related to the S32K3 Product Family. Model-Based Design Toolbox for S32K3 - Release Notes: Rev 1.6.0 - Model-Based Design Toolbox for S32K3 Automotive MCU rev 1.6.0   Rev 1.5.0 - Model-Based Design Toolbox for S32K3xx Automotive MCU rev 1.5.0   Rev 1.4.0 - Model-Based Design Toolbox for S32K3xx Automotive MCU rev 1.4.0  Rev 1.3.0 - Model-Based Design Toolbox for S32K3xx Automotive MCU rev 1.3.0  Rev 1.2.0 - Model-Based Design Toolbox for S32K3xx Automotive MCU rev 1.2.0   Rev 1.1.0 - Model-Based Design Toolbox for S32K3xx Automotive MCU rev 1.1.0  Rev 1.0.0 - Model-Based Design Toolbox for S32K3xx Automotive MCU rev 1.0.0 
View full article
    Product Release Announcement Automotive Processing NXP Model-Based Design Toolbox for S32K3xx – version 1.0.0 RTM       The Automotive Processing, Model-Based Design Tools Team at NXP Semiconductors, is pleased to announce the release of the Model-Based Design Toolbox for S32K3xx version 1.0.0. This release supports automatic code generation for S32K3xx peripherals and applications prototyping from MATLAB/Simulink for NXP S32K3xx Automotive Microprocessors. This new product adds support for S32K344 MCU and part of its peripherals, based on RTD MCAL components (ADC, PWM, MCL, DIO, CAN, SPI, GPT). It also adds support for FreeMASTER, AMMCLib, and Simulink simulation modes – Software-in-Loop, Processor-in-Loop, and External mode. Moreover, this release adds the option to configure everything (pins/peripherals/clock) via an external configuration tool - S32 Configuration Tools or EB Tresos. The product comes with over 70 examples, covering everything that is supported, including a motor control application demo. FlexNet Location: https://nxp.flexnetoperations.com/control/frse/download?element=12747097 Technical Support: NXP Model-Based Design Toolbox for S32K3xx issues will be tracked through the NXP Model-Based Design Tools Community space. https://community.nxp.com/community/mbdt   Release Content Automatic C code generation from MATLAB® for NXP S32K3xx derivatives: S32K344 Support for the following peripherals (MCAL components): ADC PWM MCL CAN SPI GPT DIO Support for profiling execution times Support for register R\W and memory R\W operations Provides 2 modes of operation: Basic User Mode – using pre-configured configurations for peripherals; useful for quick hardware evaluation and testing Advanced User Mode – using S32Configuration Tool or EB Tresos to configure peripherals/pins/clocks Integrates the Automotive Math and Motor Control Library release 1.1.24 for: All functions in the Automotive Math and Motor Control Functions Library v1.1.24 are supported as blocks for simulation and embedded target code generation.   FreeMASTER Integration We provide several Simulink example models and associated FreeMASTER projects to demonstrate how our toolbox interacts with the real-time data visualization tool and how it can be used for tuning embedded software applications.   Support for MATLAB versions We added support for the following MATLAB versions: R2020a R2020b R2021a S32Design Studio Integration We added a simple mechanism to provide users the opportunity to export the generated code from Simulink and import it directly into S32Design Studio. This functionality can be useful if the model needs to be integrated into an already existing project, as well as for debugging purposes.   Simulation modes: We provide support for the following simulation modes (each of them being useful for validation and verification): Software-in-Loop (SIL) Processor-in-Loop (PIL) External mode   Examples for every peripheral/function supported: We have added over 70 new examples, including: Motor control application Communication (SPI, CAN) AMMCLib Timer control (GPT) DIO FreeMASTER SIL / PIL / External mode MATLAB® Integration The NXP Model-Based Design Toolbox extends the MATLAB® and Simulink® experience by allowing customers to evaluate and use NXP’s S32K3xx MCUs and evaluation board solutions out-of-the-box with: NXP Model-Based Design Toolbox for S32K3xx version 1.0.0 is fully integrated with MATLAB® environment in terms of installation: Target Audience This release (1.0.0) is intended for technology demonstration, evaluation purposes, and prototyping S32K3xx MCUs and Evaluation Boards.    Useful Resources Examples, Training, and Support: https://community.nxp.com/community/mbdt    
View full article
This page summarizes all Model-Based Design Toolbox tutorials and articles related to i.MX RT Product Family Facial Recognition Application in Co-Simulation mode for IMXRT117X Sensor application for IMXRT1060
View full article
This page summarizes all Model-Based Design Toolbox videos related to i.MX RT Product Family
View full article
1.  Introduction The NXP i.MX RT1xxx Toolbox enables automatic code generation for peripherals and applications prototyping from MATLAB/Simulink for NXP’s i.MX RT 117x, 106x & 101x Series of crossover MCUs. The toolbox can be installed from Matlab add-ons page:   The novelty of this NXP toolbox is the integration with MCUX Configuration Tool for platform initialization. This configuration tool is being leveraged for pins settings, clock configuration and peripheral initialization. The toolbox is also integrated with the MCU SDK and will use the SDK API for code generation. This article details the steps to start building new models and deploy them on the i.MX RT106x, i.MX RT1010 & i.MX RT 117x MCU, showcasing also the integration with the MCUX Configuration Tool. 2.  Start creating your model Below are the steps to start creating a Simulink model that will be deployed on the i.MX RT1xxx boards. Step 1: Better to start on clean so first lets create folder to be used as workspace and switch MATLAB current folder to point to this workspace location:   Step 2: Create a Simulink Blank Model.   Step 3: Save and name your new model (E.g. mytest.slx). Step 4 : Choose the NXP IMXRT hardware board from the Model Settings in the MODELING tab.         Step 4.1: Open  Model Settings -> Hardware Implementation menu         Step 4.2: Select the NXP target from Hardware Board. This selection should match the             evaluation kit you plan to test the code for. After the selection is made, press the Apply button. After the target is set, the workspace will be populated with new files and folders: A file with extension <model_name>Config.mex – this is the file created with MCUX Configuration Tool that is used for pins, clock, and peripherals initialization. This configuration file will have enabled the peripherals that are supported by the toolbox. Starting from this, the user can change the default configuration for any of the peripheral instances (add new instances, disable instances, etc.) and also any of the configured pins.   A folder with naming pattern <model_name>Config -  this folder will have a structure that is similar to the MCUXpresso IDE projects, and will contain the SDK files that are needed to build the model and generate a binary application that will run on the board. The user can now add Simulink blocks in the model from the NXP i.MXRT1xxx Simulink library from Simulink Library Browser:   Choose the desired block to add to the model:   Alternatively, if the user will add in his/her model a peripheral block without configuring the target, a default one will be set that the user can change it afterwards.  3.  Modify default platform initializations and settings values As mentioned at the beginning of this article, the platform initialization, including pins, clock and peripherals settings is done using the MCUX Configuration Tool. As seen in the previous chapter, when a Simulink model is being created with one of the NXP IMXRT targets, the workspace will be populated with a file having the extension .mex – this is the configuration file that will be used in the initialization code of the platform. The user has the option to modify the default selections found in the .mex file. For this, open any peripheral block within the model and press the Configure button. This action will open the MCUX Configuration Tool.   From MCUX Configuration Tool, the user can change default settings of the peripherals – enable or disable instances, from Pins view, it can configure/update pins settings of the platform. After the user is done with configuration in MCUX Configuration Tool, he/she must go back in Simulink and press the Update button in the same block, for the changes to be visible in Simulink also. The new initialization settings, will be included in the Build Model step. The Toolbox will trigger a code generation starting from the .mex file. The generated files will be saved in the <model_name>Config folder, in board folder.   Note, that is not a prerequisite for the user to have MCUX Configuration Tool installed, the toolbox incorporates all the tools that are need for the user to create, configure,  build and deploy the model.  The default MCUX Configuration Tool used can be changed from Model Settings/Hardware Parameters / Tools Path, and the user can provide his/her own installation of the tool. Same approach is used with the SDK platform. The toolbox incorporates the release version of the SDK for the IMXRT1xxx targets. Also this path can be changed by the user, but it must consider possible integration issues of the toolbox with the user specified SDK.     4.  Deploy on NXP Hardware After the Simulink model is completed, follows the build and deployment of the model on the target board. Before Build and Deploy, the user must set the download method of the application. Step 1: Select the Download method from Hardware Implementation in Model Settings.   The default Download method (without the need for additional software and/or hardware probes) is OpenSDA. For this, the user must select the Drive on his/her machine where the OpenSDA firmware of the board is mapped after the NXP evaluation board is plugged in via USB. Step 2: Build & Deploy Model Step 3: After the code is generated and downloaded on the board a window will pop up and tell you to restart the evaluation board. Restart the board and then press OK. Congratulations! You have successfully created and deployed your Simulink model to the hardware.
View full article
Speed up development time with NXP Model-Based Design Toolboxes
View full article
Model-Based Design Toolbox supporting i.MX RT Crossover MCU. System modeling, simulations, automatic code generation, validation, and verification MATLAB & Simulink workflows are now available on the i.MX RT microcontroller by reusing MCUXpresso ecosystem: MCUXpresso SDK MCUXpresso Configuration Tool MCUXpresso IDE,GCC
View full article
Model-Based Design Toolbox supporting Kinetis-V Series. System modeling, simulations, automatic code generation, validation, and verification MATLAB & Simulink workflows are now available on the Kinetis V microcontrollers by reusing MCUXpresso ecosystem: MCUXpresso SDK MCUXpresso Configuration Tool MCUXpresso IDE,GCC
View full article
      Product Release Announcement Automotive Processing   NXP Model-Based Design Toolbox   for S12ZVMx – version 1.4.0     Austin, Texas, USA September 9, 2020 The Automotive Processing, Model-Based Design Tools Team at NXP Semiconductors, is pleased to announce the release of the Model-Based Design Toolbox for S12ZVMx version 1.4.0. This release supports automatic code generation for S12ZVM peripherals and applications prototyping from MATLAB/Simulink for NXP S12ZVMx Automotive Microprocessors. This new release adds extended MATLAB version support (R2015a-R2020a), integrates with AMMCLib v1.1.21, is compatible with MathWorks Automotive Advisory Board checks, adds over 50 new examples and more.   FlexNet Location: https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=MCTB-EX   Activation link: https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=MCTB-EX   Technical Support: NXP Model-Based Design Toolbox for S12ZVMx issues are tracked through NXP Model-Based Design Tools Community space. https://community.nxp.com/community/mbdt   Release Content Automatic C code generation from MATLAB® for NXP S12ZVMx derivatives: S12ZVM 32/L31/16: MC9S12ZVM16 MC9S12ZVML31 MC9S12ZVM32 S12ZVML/C 128/64/32: MC9S12ZVML32 MC9S12ZVML64 MC9S12ZVMC64 MC9S12ZVML128 MC9S12ZVMC128 S12ZVMC256: MC9S12ZVMC256   Integrates the Automotive Math and Motor Control Library release 1.1.21: All functions in the Automotive Math and Motor Control Functions Library v1.1.21 are supported as blocks for simulation and embedded target code generation for: Bit Accurate Model for 16-bit fixed-point implementation Bit Accurate Model for 32-bit fixed-point implementation Bit Accurate Model for floating-point single precision implementation             Extended support for MATLAB versions We extended support for our toolbox to cover a wider range of MATLAB releases – starting from R2015a and going up to R2020a. This way we want to avoid locking out users that have constraints regarding MATLAB versions. Motor control examples We have added new motor control examples – BLDC (closed loop) and PMSM (closed loop, sensorless):   MAAB Checks (MathWorks Automotive Advisory Board) The toolbox is compatible with MathWorks Automotive Advisory Board checks – reports can be generated from Model Advisor:   Updated examples: We have added over 50 new examples, including: Motor control (both BLDC and PMSM) AMMCLib GDU (Gate Drive Unit) Profiler For more details, features and how to use the new functionalities, please refer to the Release Notes document attached.   MATLAB® Integration The NXP Model-Based Design Toolbox extends the MATLAB® and Simulink® experience by allowing customers to evaluate and use NXP’s S12ZVMx MCUs and evaluation boards solutions out-of-the-box with: NXP Support Package for S12ZVMx  Online Installer Guide Add-on allows users to install NXP solution directly from the Mathwork’s website or directly from MATLAB IDE. The Support Package provide a step-by-step guide for installation and verification. NXP Model-Based Design Toolbox for S12ZVM version 1.4.0 is fully integrated with MATLAB® environment in terms of installation: Target Audience This release (1.4.0) is intended for technology demonstration, evaluation purposes and prototyping S12ZVMx MCUs and Evaluation Boards.   Useful Resources Examples, Trainings and Support: https://community.nxp.com/community/mbdt                                                    
View full article
This article details the TPL communication setup between S32K1xx boards and MC3377xBTPL Battery Cell Controllers.  It covers both hardware and software setup for the Battery Management System models designed using Model-Based Design Toolbox for battery packs of more than 14 cells in series.  At the end of this article, the user will be able to setup the Battery Cell Controller hardware and to design a Simulink model that reads the cell and pack voltages, current, temperatures and faults status. The measured values will be displayed on the host PC using FreeMaster. 
View full article