NXP Model-Based Design Tools Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXP Model-Based Design Tools Knowledge Base

Discussions

Sort by:
Check this short video to see the cool stuff you can do with an S32K144 DevKit. NOTE: Chinese viewers can watch the video on YOUKU using this link 注意:中国观众可以使用此链接观看YOUKU上的视频
View full article
In this video we show the hall pattern identification procedure that can be applied to any motor in case you have no datasheet available. We will read the hall sensors outputs via the microprocessor and save the information for later use.   We show: - How to prepare the Hardware setup - How to go over each identification table - row by row - to apply DC voltage and rotate the rotor in different sectors 360 degrees. NOTE: Chinese viewers can watch the video on YOUKU using this link 注意:中国观众可以使用此链接观看YOUKU上的视频
View full article
This video is part of the https://community.nxp.com/thread/467938  Workshop module and shows how to implement a simple V/F (V/Hz) scalar control to spin the PMSM in open loop using Space Vector Modulation and trapezoidal speed profile.
View full article
In this video we discuss about how the motor phase commutation works. This is an essential topic to understand how the motor rotates based on 6-step commutation technique.   We discuss about: - How to build the commutation table based on hall pattern identification  - How to control the PWM sequence to implement a 6-step/trapezoidal commutation NOTE: Chinese viewers can watch the video on YOUKU using this link 注意:中国观众可以使用此链接观看YOUKU上的视频
View full article
This video is part of the Module 7: Torque Control  Workshop module and shows how to implement a FOC and control the PMSM torque and flux using standard PI controllers. This method is used to spin the PMSM in open loop using Space Vector Modulation. The video shows how to implement a control system with two control loops: FAST and SLOW
View full article
In this video we implement Simulink models for reading the hall sensors directly via GPIO or based on Hall transitions interrupts via eTimer Capture.   We discuss about: - How to build simple hall reading application using the available MBD Toolbox GPIO blocks  - How to enhance this simple model by adding interrupt service routines capabilities to read the hall sensors only when there is a transitions - How to count the number of hall transitions - How to validate the applications with FreeMASTER NOTE: Chinese viewers can watch the video on YOUKU using this link 注意:中国观众可以使用此链接观看YOUKU上的视频
View full article
In this video we talk about  how hall sensors works, how the commutation sectors are defined based on hall transitions and how can we identify the hall patterns when no datasheet is available.   We discuss about: - Hall sensors - Commutation sectors  - Hall sensors alignment procedure - Hall sensors electronic circuit used on MotorGD and MPC5744P devkits NOTE: Chinese viewers can watch the video on YOUKU using this link 注意:中国观众可以使用此链接观看YOUKU上的视频
View full article
In this video we discuss about how to use Software-in-the-Loop (SIL) approach to generate the C-code for the first time and validate the algorithm at the concept level.   We discuss about: - What is SIL, When to use it and What is recommended for;  - How to convert any Simulink generic algorithm to run with SIL support using the Model Based Design Toolbox; - SIL Reference models;  NOTE: Chinese viewers can watch the video on YOUKU using this link 注意:中国观众可以使用此链接观看YOUKU上的视频
View full article
In this video we talk about  different motors classification, BLDC motor modelling and how to control the BLDC rotor movement.   We discuss about: - How most common motors operates - Electro-mechanical equations of BLDC motor - How BLDC works - Practical implementation of commutation sequence - BLDC vs PMSM comparison NOTE: Chinese viewers can watch the video on YOUKU using this link 注意:中国观众可以使用此链接观看YOUKU上的视频
View full article
This video discuss about how to mix together the ADC and GPIO models to obtain a common speed reference for the BLDC speed closed loop control system.   We discuss about: - How to use analog and digital inputs - How to create a variable that can be changed in real time via Freemaster - How to test the final application - Finalize the Speed Reference Block - Short Quiz NOTE: Chinese viewers can watch the video on YOUKU using this link 注意:中国观众可以使用此链接观看YOUKU上的视频
View full article
This video shows how to program the GPIO with Model Based Design Toolbox to obtain the speed reference for the BLDC speed closed loop control system.   We discuss about: - How to implement a simple program to read data from the GPIO - How to test in real time with FreeMaster - How to transform GPI pulses into a speed reference data that represents the rpm. - How to implement from scratch a Simulink model to cover the GPIO functionality NOTE: Chinese viewers can watch the video on YOUKU using this link. 注意:中国观众可以使用此链接观看YOUKU上的视频
View full article
This video shows how to program the ADC with Model Based Design Toolbox to obtain the speed reference for the BLDC speed closed loop control system. We discuss about: - How the ADC works - How to simulate the ADC operations - How to implement a simple program to read data from the ADC - How to use BAM to load the application into microprocessor memory - How to test in real time with FreeMaster - How to scale the Potentiometer voltage into a speed reference data that represents the rpm. - How to implement from scratch a Simulink model to cover the ADC functionality NOTE: Chinese viewers can watch the video on YOUKU using this link. 注意:中国观众可以使用此链接观看YOUKU上的视频
View full article
This video shows how to navigate within the integration Matlab help for NXP's Model-Based Design Toolbox for S32K1xx. The following items will be highlighted: Getting HELP Open Examples Support via Community
View full article
This video explains how to use a three phase inverter to control the voltage applied on PMSM using various PWM Modulation techniques like: bipolar modulation unipolar modulation sinusoidal modulation space vector modulation third harmonic injection The goal of this video is to cover the topic of Space Vector Modulation and PWM generation that represents the basics for applications we are going to develop throughout https://community.nxp.com/thread/464336 .
View full article
This video shows how: Install the Support Package Add-On Use of Installer Wizard Toolbox package download & install License generation and setup
View full article
A short - 1 minute - Motor Control Class introduction that highlight the main topics and objectives of the training series NOTE: Chinese viewers can watch the video on YOUKU using this link. 注意:中国观众可以使用此链接观看YOUKU上的视频
View full article
This video presents the hardware and software setup used for Motor Control Class. It shows: - MPC5744P DevKit main hardware features - MotorGD DevKit main hardware features - How to install the Model Based Design Toolbox for MPC5744P revision 2.0.0 - How to generate a license - How to setup a compiler toolchain using S32 Design Studio for Power Architecture - How to add the Model Based Design Toolbox for MPC5744P into the Simulink Standard Libraries - How to validate the software installation by generation C code for the first time NOTE: Chinese viewers can watch the video on YOUKU using this link. 注意:中国观众可以使用此链接观看YOUKU上的视频
View full article
This video presents the system block diagram for BLDC speed closed loop control and how to map the application block diagram over the existing hardware. We discuss about: - What is a BLDC motor and how is made - How a BLDC motor works with electronic commutation - What is needed to construct a speed control loop - Mapping the SW and HW together NOTE: Chinese viewers can watch the video on YOUKU using this link. 注意:中国观众可以使用此链接观看YOUKU上的视频
View full article
This video shows the main differences between basic and advanced modes for peripheral configuration
View full article
This video shows how easy it is to build a motor control application for BLDC with NXP's Model-Based Design Toolbox
View full article