NXP FTF 2016 - Training Presentations

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXP FTF 2016 - Training Presentations

Discussions

Sort by:
This presentation will cover the Hardware Security Module (HSM) and how to use the software kits NXP offers, the HSM Security Firmware and HSM Software Development Kit. We will also cover other security features of the device offered by modules like PASS or TDM and their configuration. Watch Video Presentation
View full article
As the 5G standard is being defined, high throughput, low latency and a high number of users are among the key requirements to drive 5G services. See how NXP is blending these ingredients to design an optimal hardware architecture to address the challenges of 5G.
View full article
Get up and running in minutes with the NXP S32K platform using the S32 SDK and S32 Design Studio. This hands-on session will introduce the full flexibility and capability of the S32 SDK package, outlining the excellent out-of-the-box experience, ease of use and shorter time to market. Attendants will learn how to use it in correlation with S32 Design Studio IDE to quickly create suitable applications for general-purpose use-cases, running through all the development steps (installation, software configuration & RTOS integration, inserting application code and target debug).
View full article
The standard CAN protocol has been extended into CAN Flexible Data (FD) to provide higher bandwidth while keeping the physical characteristics that have made it the most popular automotive in-vehicle communications protocol . This presentation will provide an overview of the changes to the standard as well as address the challenges faced while rolling out and implementing the technology. Watch Video Presentation
View full article
The session will consider the use of discrete power MOSFETs in automotive applications such as powertrain, safety, chassis and body control, guiding attendees to the best choice of NXP’s latest silicon and packaging technology. Solutions for motor control for fuel, oil, and water pumps will be highlighted. Watch Video Presentation
View full article
Many customers struggle getting their first GUI design running, and often this results in schedule and budget problems. This class covers the issues and SOLUTIONS required to get a Graphical User interface up and running. We provide solutions to standard embedded communication requirements like Ethernet, USB, Wi-Fi, and Serial. We present a Case Study of a new product using a touch screen GUI, LEDs and audio to communicate the fluid level and temperature of a beverage container back to the user. We cover the pros and cons of developing your own software or of using proven off-the-shelf solutions based on standard building blocks. We also address the buy vs. make hardware decision and look at time to market and risk factors. The class ends with a demonstration of the solution implemented with an off-the-shelf NXP LPC microcontroller based hardware module and simple custom expansion board.
View full article
The two big topics in automotive electronics development in the last five years has been functional safety and security. Sometimes these terms are used synonymously, sometimes completely separately. This thought provoking presentation will explore where the two topics overlap, where they result in contradictory requirements, and indeed whether they are complementary. Watch Video Presentation
View full article
The hottest topic in automotive design today is the concept of the eCockpit -- where all visual functions in the car are controlled across multiple screens and fully integrated for the driver’s convenience. The key technology that enables eCockpit to run on a single processor also offers new capabilities in industrial, embedded and consumer products such as drones, manufacturing HMI interfaces and smart displays. This class will cover the fundamental technologies and architectural techniques in the i.MX 8 processor which enables rich eCockpit functionality, how NXP has implemented the world’s most significant full chip virtualization capabilities in an ARM-based processor and breaks down the eCockpit demo from the Tech Lab.  Watch Video Presentation
View full article
Learn about the exciting new Network Function Virtualization use case driving enterprise OEMs and service provider Cloud and premises architectures. Understand the new NXP open standard and optimized NFV system solutions which offers best performance-per-watt. And realize how this NFV software suite, combined with NXP processors, will protect customer CAPEX/OPEX, speed deployment time to market and enable new customer revenue streams.
View full article
This session will present the structure of NXP Yocto layers and mechanism of software delivery. Various architectures (ARM®v7, ARM®v8 and PPC) can be supported, the common software components can be shared by different products (i.MX and QorIQ processors) via the unified NXP Yocto layer which manages the free software and maintained by Yocto community. The commercial software can be delivered via separated layers, QorIQ LS2 SDK is using the mechanism for commercial software delivery, e.g. nsp, openflow, ssp and tcpoffload. The session also introduces how to create Yocto layer for customization changes and commercial products. Watch Video Presentation
View full article
This session discusses how the i.MX applications processors interface with the new NXP portfolio. We will review the i.MX processor family and how they can be connected to NXP components to create complete automotive platforms. Watch Video Presentation
View full article
Explore the NXP wearable and fitness product roadmap and solutions platform. Watch Video Presentation
View full article
DDR3, DDR3L, DDR4 have large, wide busses that require management on the PCB routing to optimize their speed of operation. Data busses will have characteristics related to on-die termination and driver strengths for both reads and writes (bidirectional). Address-Command-Control busses will be use the fly-by or serial routing and work unidirectionally. Both require careful selection of driver and receiver characteristics, as well as optimization of the PCB routing and design of the traces on the PCB. This talk will review the driver, receiver, and common PCB characteristics and show how simulation with IBIS models are used to weigh the trade-offs for the DDR bus design. Watch Video Presentation
View full article
This will be a hands-on session covering the Kinetis Software Development Kit (SDK) and Kinetis Expert using the Kinetis Design Studio Integrated Development Environment (IDE).  
View full article
Learn how NXP's Motor Control reference design and control libraries, built on the Kinetis V portfolio, can help you beat deadlines, improve your time to market, and achieve better motor performance. In this hands-on class you will learn how to use NXP's complimentary reference designs and control libraries to get to market quicker with better designs.
View full article
Whether your requirements are size and power, or range and bandwidth, there is a right-sized Wi-Fi solution available now for your i.MX-based processor design! Through partnerships with industry leaders in Wi-Fi technology and module design, NXP can now offer proven Wi-Fi solutions across a range of size, power and performance levels suitable for consumer, automotive, industrial and battery-powered mobile or remote i.MX-based applications. In this session we will cover the latest Wi-Fi protocols, certifications, and interoperability issues for Wi-Fi, as well as the range of wireless LAN solutions now available for use with i.MX applications processors and evaluation boards. Watch Video Presentation
View full article
This hands-on class will walk you through developing two separate applications. First, learn how to leverage a FlexIO driver to add some autonomous monitoring and reaction to sensor data. Secondly, learn how to create a complex parallel interface (TFT driver).
View full article
With 5G solutions still being in the design phase, NXP delivers RF solutions based to meet the growing data demand. These solutions are called 4.5G and are based on smart combinations of existing 4G and Wi-Fi technology and will enable a high throughput internet connections everywhere on this planet. This lecture will show you the existing 4G and Wi-Fi RF solutions and how they can be utilized for 4.5 G networks and which steps need to be taken to bring these solutions towards the 5G network. Watch Video Presentation
View full article
In designing cooking appliances, there is ample consideration given to power required from a home's wired electrical system as well as the performance needed to maintain safety and operating temperatures. NXP's solid state RF cooking team has partnered with Wayv Technology to develop a portable food heating appliance using solid state RF energy. This session will cover the key challenges and approaches to delivering energy to heat food in a portable, on-the-go appliance. Watch Video Presentation
View full article
Today’s designers are facing ever increasing challenges to protect their intellectual property and products from counterfeiting or unauthorized access. To help customers better understand the solutions offered by NXP, Future’s System Design Center has designed a Secure Access Demo board to showcase the capabilities of the LPC43S57, a microcontroller with integrated security, and the A700X, a tamper resistant secure MCU solution. This class will present an overview of the architecture of a secured system and provide an introduction to the secured elements from NXP. Watch Video Presentation
View full article