NXP FTF 2016 - トレーニングプレゼンテーション

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NXP FTF 2016 - Training Presentations

ディスカッション

ソート順:
With the introduction of MIFARE Plus® EV1 NXP enables universities currently using MIFARE Classic to introduce latest technology in the existing system, upgrade the security of applications depending on their needs and complement daily use cases with mobile devices. Through the option to upgrade individual applications of your system fast security upgrades for critical applications are possible whereas non-critical applications remain in the existing mode without any changes. MIFARE Plus EV1 further includes the option to complement existing applications with mobile use cases. Through its enhanced possibilities MIFARE Plus EV1 based cards can now easily be integrated in cloud applications while maintain banking grade security.
記事全体を表示
Embedded Planet designed the new NXP LS1043 Gateway. Come learn the details of the hardware and software designed for this next generation residential Gateway.
記事全体を表示
Using Accelerometers, Magnetometers, Gyroscopes, gathering Sensor data can be tricky and not straight-forward. In this class, we will go into a Sensor Deep-Dive, where each sensor will be visualized and explained in detail. When collecting data there are several things that can make collecting the data easier, more efficient, and avoiding erroneous data all together. We will have several demonstrations and examples to show the pitfalls and successes of collecting data.
記事全体を表示
This paper will examine the use of an i.MX 6 IOT Gateway working together with a Cloud Services Platform (CSP), to collect and transmit data from a temperature sensor. The design options for seamless data transmission from device, to gateway, to cloud and then to a hand-held Smartphone will be considered and presented using Mentor Embedded Linux, Nucleus as well as Cloud Service Platforms.
記事全体を表示
This session will provide an overview of the QorIQ's hardware root of trust, key protection, and strong partitioning capabilities. Watch Video Presentation
記事全体を表示
FIDO Alliance is getting huge traction in the secure authentication world and the member count has surpassed 250 companies. Secure Element based FIDO U2F Authenticators add another security layer to consumer online authentication for cloud services and have been deployed for services like Google, Dropbox, Github, and others. These Authenticators are available in various form factors (Cards, USB keys, Fobs, Wearables and embedded) and support multiple interfaces like USB, NFC and BLE to connect users to critical online services using the FIDO authentication protocol. In addition to FIDO credentials, NXP provides vSE based multi-credential (PKCS#15, EAC, BAC, SAC, Mifare, PIV ) as well as an online services platform including eDoc derived mobile credential management connecting relying parties to enable secure mobile authentication for eGov services. Watch Video Presentation
記事全体を表示
Transport ticketing requirements have evolved significantly over the last years - from transaction security to multi-application needs and the possibility to integrate mobile ticketing to an existing environment. NXP's MIFARE® products have consistently been able to meet these requirements and strongly establish an excellent reputation as the leading contactless solution delivering convenience, flexibility and scalability. Over 1,000 business partners including application developers, service and solution providers, system integrators and card manufacturers make up the open MIFARE community and ecosystem. MIFARE DESFire EV2 is the next-generation of MIFARE ICs with highest security level (EAL5+ Common Criteria certification) for hardware and software. Its enhanced key management makes it the ideal multi-application platform for unlimited applications.
記事全体を表示
ODP and DPDK are open-source project that defines a standard set of APIs for data-plane to be used across the different network processor architectures. This session details how the standard DPDK and ODP APIs are being mapped to NXP data-path acceleration for specific packet processing elements (packet IO, classification, scheduling, crypto, etc.). It also propose various possible API extensions to get additional performance on NXP SoCS. This presentation will cover how the ODP and DPDK can provide the necessary infrastructure for virtualized environments.
記事全体を表示
Smart digitalized packaging as a subset of the Internet of Things - a huge trend impacting global packaging industry today. NXP is the Identification industry's #1 chip supplier for smart secure NFC-RFID technology offering a variety of tag ICs from short to long-range, allowing interaction with mobile phones connecting products to the cloud and customers to brands. Watch Video Presentation
記事全体を表示
Many people involved in the electronics industry need a basic knowledge of semiconductor components in order to understand issues like manufacturing cycle time, semiconductor fab consolidation and failure analysis results. This session is geared towards a non-technical audience and gives a high-level overview of semiconductor devices and how they are made. The lecture begins with a brief overview of how semiconductor devices work. The bulk of the presentation describes the generic manufacturing flow for semiconductor devices with an emphasis on the complexity of the equipment/facilities used and the process time required. Watch Video Presentation
記事全体を表示
This session will provide tips that will help speed up silicon bring up of the QorIQ LS1043A processor.
記事全体を表示
The session will provide an overview of the most recent developments to support Radar systems in the frequency range from 76 GHz up to 81 GHz. High level block diagrams and key specifications of NXP multi-channel transceivers will be presented. It will also be discussed how the NXP transceiver solutions can help to enable modern low power consumption sensors with robustness against frequency interference, small size, and high-performance due to scalability. In combination with NXP Radar micro-processors and mircro-controllers typical Radar system architectures will be introduced. Especially for the development of small and compact cocoon, nano radar sensors an example is presented which shows the combinations of NXP Radar tranceivers, NXP Radar processors and NXP power supply solutions. The presentation will also give an outlook to technology trends and future upcoming NXP Radar solutions.
記事全体を表示
The AIOP C programmable packet engine is a fundamental component of the Data Path Acceleration Architecture (DPAA2). It provides customers with an opportunity to achieve the best performance per watt solution, by offloading routine packet processing tasks to the AIOP packet engine, while doing more complex processing on the ARMv8 cores. This sessions explores how customers can get to fast time-to-market with high performance, commercial grade acceleration packages from NXP.
記事全体を表示
Building on top of 11 years of usage within data centers, Xen Hypervisor is uniquely placed to support a new range of use cases for embedded solutions. In particular, its isolation and security features, flexible virtualization modes and architecture, driver disaggregation, and strong ARM support make it a perfect fit for embedded applications. Artem Mygaiev, GlobalLogic’s Embedded Practice Head, will explore the virtualization nuances and challenges of using Xen Hypervisor for embedded applications through the demonstration of his own company’s journey in developing a platform that leverages Xen for virtual network equipment, IoT, automotive, and other embedded use cases.
記事全体を表示
Networking devices use high-speed differential signaling that can exceed 10 Gbps. Circuit design for the transmitter (TX) and receiver (RX) elements in the high speed channel have capabilities of offset signal losses in the PCB and system. This session will review the high-speed signal channel and its characteristics and illustrate how the TX and RX circuits in general are used to offset signal losses. It will also show key characteristics of the channels that are needed to allow these TX and RX circuits to work effectively. This session will also address maximum length of the PCB channel, PCB-specific structures that need to be optimized and the usage of the IBIS-AMI models for 5-10 Gbps operation. Examples of channels from PCB designs at NXP will also be included. Watch Video Presentation
記事全体を表示
Cars depend on a range of systems that must guarantee safety for their drivers. Linux and Open Source have already entered the infotainment segment, but expanding to ADAS presents new challenges with regards to safety and change control. This session will provide an overview of the internals of the kernel, the safety-critical components, implementation of fault recovery mechanisms and finally how open source software can be used for Autonomous Drive applications. Watch Video Presentation
記事全体を表示
With new CAN FD protocol, CAN applications need to support both classical CAN and CAN FD frames. Especially in transition period, customers are looking for a solution in which classical CAN frames are mixed with CAN FD frames. NXP developed a brand new CAN transceiver feature "CAN FD Shield", which enables the use of CAN controllers in mixed CAN / CAN FD architectures. Watch Video Presentation
記事全体を表示
The RF content of connected devices has been increasing dramatically the last couple of years. The increasing bandwidth demand has driven the requirements of the RF chain to higher levels. The RF MMICs from NXP Smart Antenna Solutions give designers of connected devices freedom of antenna placement while achieving higher performance. This class will show the increasing requirements and complexity and NXPs answer to this challenge. Watch Video Presentation
記事全体を表示
This technical lecture presents how Toradex built a balancing robot demo application using the new i.MX 7's heterogeneous asymmetric architecture. i.MX 7 features a secondary Cortex-M4, which can be used for real-time or low-power applications. We will discuss how to make use of the secondary core with a FreeRTOS based firmware implementing the closed loop controller to keep the robot balanced upright. On the powerful main CPU complex, a dual Cortex-A7, Linux is running a Qt based user interface. We will go into details about the rpmsg/OpenAMP based messaging offerings provided by NXP. The robot demo application makes use of rpmsg to communicate between the two independently running processor cores and operating systems.
記事全体を表示
Companies and consumers alike are excited about the opportunities offered by the IoT and the Smart Home. Concerns on user-friendliness and security are however holding potential customers back: how can I install it? , what if my neighbor hacks into my network? NFC technology addresses these cost, ease of use and security concerns by offering short distance out-of-band pairing capabilities that reduce the complex commissioning system to a simple 'tap'. And with NXP's connected NFC tag technology, IoT nodes of all sizes do not even need to be powered. Watch Video Presentation
記事全体を表示