SMI-N2027 Toradex- A Balancing Robot Leveraging the Heterogeneous Asymmetric Architecture of i.MX 7 with FreeRTOS and Qt

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SMI-N2027 Toradex- A Balancing Robot Leveraging the Heterogeneous Asymmetric Architecture of i.MX 7 with FreeRTOS and Qt

SMI-N2027 Toradex- A Balancing Robot Leveraging the Heterogeneous Asymmetric Architecture of i.MX 7 with FreeRTOS and Qt

This technical lecture presents how Toradex built a balancing robot demo application using the new i.MX 7's heterogeneous asymmetric architecture. i.MX 7 features a secondary Cortex-M4, which can be used for real-time or low-power applications. We will discuss how to make use of the secondary core with a FreeRTOS based firmware implementing the closed loop controller to keep the robot balanced upright. On the powerful main CPU complex, a dual Cortex-A7, Linux is running a Qt based user interface. We will go into details about the rpmsg/OpenAMP based messaging offerings provided by NXP. The robot demo application makes use of rpmsg to communicate between the two independently running processor cores and operating systems.

ラベル(1)
添付
評価なし
バージョン履歴
最終更新日:
‎05-25-2016 09:52 AM
更新者: