NXP FTF 2016 - 培训演示

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

NXP FTF 2016 - Training Presentations

讨论

排序依据:
This presentation will demonstrate the capabilities of the new i.MX 7 System-on-Chip, a hybrid solution containing a Cortex-A7 processor and a Cortex-M4 processor. Particular attention will be given to the hardware modules and software counterparts allowing both cores to communicate with each other. This hybrid architecture will be highlighted through various potential use cases/product scenarios and a Qt powered application running on top of Linux along with FreeRTOS will be showcased, focusing on asymmetric processing.
查看全文
NXP’s latest generation of passive UHF RFID, called UCODE® DNA, can be used in Automatic Vehicle Identification (AVI) systems that make it easier to identify – and collect from – drivers of vehicles that aren’t properly registered. In an AVI system for vehicle registration, readers can be installed above, below, or to the side of the road. They can also be embedded in a handheld device, for use by government personnel. The tag, attached to the vehicle, uses the energy produced by the reader’s RF field, so there’s no need for a battery and the tag has a very long lifespan. Cryptography-based security minimizes errors and practically eliminates fraud. Vehicle owners (and fee collectors) can be confident that the right person is being billed, since readings are both highly accurate and highly secure.
查看全文
This session will cover emerging trends in crypto acceleration APIs, their benefits, and NXP's roadmap for supporting them. Watch Video Presentation
查看全文
Learn how NXP's Motor Control reference design and control libraries, built on the Kinetis V portfolio, can help you beat pressing design deadlines, improve your time to market, and achieve better motor performance.
查看全文
The Influencers Summit brings some of the smartest and most influential people together to openly share, debate, and learn from one another. The session provides a panel discussion with experts, followed by an opportunity for attendees to participate in roundtable discussions with IoT Security influencers. Topics that will be covered include: What plans are in place for regulating IoT activity? What needs to be done to ensure Security and Privacy concerns do not hinder future developments and deployments of IoT? How do attackers compromise connected devices? What will it take for the technology and business to make it a success? How will we know when we are there?
查看全文
Combining traditional MCU features with high voltage analog components in a single chip saves you system cost. An integral solution that improves quality and reduces footprint. This is an overview of the S12 MagniV MCU family for closure solutions such as window lift, sunroof, and sliding doors.
查看全文
This session will cover a number of topics relevant to all IoT systems and presented because of instructor’s involvement with the IPSO Alliance. The overriding goal of this session is to help prepare you to design your IoT system starting with the device, up to the Cloud and all the other required components. This session describes the IP protocols dedicated to IoT because it helps shape the system capabilities. This demo will use MQTT in conjunction with the Amazon AWS IoT service. IoT systems are made of multiple components. The most visible ones are the Cloud/web tools. In the demo, the activities are structured around the IT services that differentiate products. The Cloud services that will be covered in the session included in addition to data storage rules and actions, web visualization, and analytics. The demo code and Cloud accounts will be available to participants.
查看全文
ARM® mbed™ OS is an open source embedded operating system designed specifically for the "things" in the Internet of Things (IoT). It includes all of the features you need to develop a connected product based on an ARM Cortex-M microcontroller, and is ideal for applications in smart cities, smart homes and wearables. Fast track your IoT application development with mbed OS and it's implementation on Kinetis MCUs.
查看全文
A temperature monitoring solution permits logging of transport conditions of each individual drug package at any point in time. Patients and healthcare professionals can confirm the drug quality at the moment of administration. An easy-to-use solution will be presented that helps meet these critical requirements. It comprises a battery, an antenna and a single chip NHS3100 that integrates a sensor, clock, storage and NFC connectivity. Easy-to-use and intuitive, this solution supports wireless communication with a smart phone. It can be used for temperature monitoring of any perishable goods (like flowers, wine, food, resins, ...) as well.  
查看全文
NFC is part of the ongoing transition to connected devices. A variety of unique applications can benefit from this seamless proximity communication technology. This class is an introduction on integrating NFC and understanding the design challenges of a wireless application. To demonstrate how NFC is unique in the way it uses energy, this class will showcase an energy harvesting “Smart label” example using solar and NFC as power.
查看全文
Unified Extensible Firmware Interface (UEFI) provides a standard, modern environment for booting an operating system and running pre-boot applications. UEFI is already extensively used across the server, mobile and embedded market and supports multiple architectures (x86, ARM®) and has support for booting multiple OS (like Windows®, Linux, Mac). This session describes the UEFI bootloader on QorIQ LS series processors (LS1043A board) and how we can migrate from U-Boot bootloader to the UEFI bootloader on the LS processors. This session also showcases how it can be used to boot an CentOS Distribution using GRUB2 bootloader. For loading the CentOS kernel and RFS images we demonstrate PXE boot (Boot over Network) method. So essentially this session showcases a standard chained bootloading architecture which is extensively used to support embedded distributions like CentOS, Ubuntu, ONIE etc. Watch Video Presentation
查看全文
Learn the basics of DDR4 and how to configure the DDR4 controller on QorIQ devices. Watch Video Presentation
查看全文
Ultra Wide Band (UWB) is just about to enter the automotive space. UWB in automotive NXP enables new convenience and functional safety use cases and an increased level of security. In this session we will discuss UWB - RF technology used in the automotive domain, specifically for secure car access systems. We provide an overview of customer needs and explain advanced features and the potential of this brand new NXP solution. Watch Video Presentation
查看全文
This session will discuss various initiatives underway at the multicore association such as multicore programming practices, API design, open source multicore technology development, etc. Watch Video Presentation
查看全文
NFC enables new interfaces and use cases in the Automotive domain, such as car access and start, vehicle personalization, quick and easy connectivity and secure payment. In this session we will cover NFC working principles, NFC enabled use cases, like smartphone vehicle access and secure simple pairing, and the challenges for NFC in Automotive applications. A demo will illustrate the working principles of NFC based car access. Watch Video Presentation
查看全文
This sessions explores the information often hidden in sensor data. By using advanced statistical processing and machine learning algorithms, engineers can mine sensor data for contextual information, failure prognostics, and/or create smarter appliances.
查看全文
There is an increasing number of high/ultra high speed drives required by the industry. The theory offers the rules how to drive fast motors, however not all them are easily applicable in the real word. The significant issue is that the rules requires a pretty powerful device to be enough fast to control fast motors. The presentation offers the comparison of the theory with the experiences out of the customer project targeting the high speed motors controlled by a less powerful devices, where the less powerful controller is a pretty challenge within the overall task.
查看全文
As consumers embrace the ease-of-use and convenience of contactless payment, global retailers continue to invest in electronic mPOS solutions, with the market projected to grow to more than 80 M installed units by 2018 (IHS Research). mPOS equipment manufacturers need technology designed to address this growth, while meeting security and battery life requirements of the latest mobile payment technologies. The Tower POS development tool (TWR-POS-K81) showcases the capabilities of the Kinetis K81 microcontroller along with the expandable tower system, including the latest NFC controller PN5180 as well as a contact reader interface (TDA8035). A demo application is showing the EMVL1 functionality for NFC and contact transactions. Development tools will be available for all participants of this sessions. Watch Video Presentation
查看全文
DDR3, DDR3L, DDR4 have large, wide busses that require management on the PCB routing to optimize their speed of operation. Data busses will have characteristics related to on-die termination and driver strengths for both reads and writes (bidirectional). Address-Command-Control busses will be use the fly-by or serial routing and work unidirectionally. Both require careful selection of driver and receiver characteristics, as well as optimization of the PCB routing and design of the traces on the PCB. This talk will review the driver, receiver, and common PCB characteristics and show how simulation with IBIS models are used to weigh the trade-offs for the DDR bus design. Watch Video Presentation
查看全文
Trusted Platform Modules (TPMs) are standards based hardware roots of trust with protected key storage. This session covers how QorIQ Trust Architecture primitives can be used as Soft TPM, thereby reducing BOM cost by eliminating a discrete TPM chip.
查看全文