NXP FTF 2016 - Training Presentations

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXP FTF 2016 - Training Presentations

Discussions

Sort by:
This session will highlight the advantages of Bluetooth® smart mesh technology for the Internet of Things (IoT). It will focus on the ease of use and low cost of deployment of a mesh network in IoT applications, using an interactive smart mesh implementation on Kinetis KW41Z MCU as a demo vehicle, thus helping demonstrate how this device is an ideal solution for smart mesh customers.
View full article
Designing solid state RF solutions to deliver controllable, high efficiency energy for consumer cooking appliances requires designers to carefully consider size, cost, and performance objectives. This session will cover NXP's approach to a scalable, modular platform for delivering controllable RF energy for integration into cooking appliances. Watch Video Presentation
View full article
Embedded system developers often have the impression that adding wireless connectivity to a device is a “black art,” only suitable to be performed by hardware and software wizards. We'll provide an overview of the challenges to overcome when building connected devices. We'll show how GainSpan wizards have made adding wireless connectivity to NXP-based MCUs an easy task suitable for any muggle. We will showcase GainSpan’s easy-to-use Wi-Fi modules and features of the built-in networking stack and services that take the difficulty out of adding wireless connectivity to an embedded design using NXP MCUs by demoing wireless connectivity using the Kinetis SDK, i.MX Application processor platforms and LPCXpresso-based development board. Audience will leave the session with the knowledge and motivation to get started on integrating wireless connectivity into their next NXP-based embedded design.
View full article
For the Internet of Things (IoT) in the home to become a reality, companies need an open ecosystem approach that addresses all aspects from the IPv6 based mesh networking protocol to the end user experience. This class will explain how Thread fits into the smart home landscape, the key benefits Thread provides and how to take your Thread product concept from an idea to a product in the market using building blocks provided by NXP and other resources in the Thread ecosystem. Watch Video Presentation
View full article
Solid state RF energy provides cooking appliance OEMs the opportunity to create differentiated cooking appliances. When combined with emerging food services, these appliances can enable greater levels of consumer convenience while delivering consistent cooking results. This session will cover the underlying basics of how solid state RF cooking is performed, its benefits, and how it can be combined in an IoT appliance to deliver even further differentiation. Watch Video Presentation
View full article
This session will provide an introduction to developing Made For iPod (MFi) accessories including audio, non-audio, CarPlay, AirPlay and HomeKit applications based on NXP microcontrollers (MCUs), microprocessors (MPUs), HomeKit Software Development Kit (SDK), MFi SDK, and software from NXP Professional Services.
View full article
The course will detail RFC 7668 (6LoBLE), Bluetooth® low energy 4.2 and the Internet protocol support profile that are used to transport IPv6 frames in an IoT environment. The demo will be based on the Kinetis KW41 MCU.
View full article
Brillo is a lightweight OS based on Android for connected devices with a small footprint that is open, extensible and secure. Brillo extends the Android platform to all your connected devices so they are easy to set up and work seamlessly with each other and your smartphone. It comes with 'Weave' Googles communication API, which easily allows Brillo devices to communicate and exchange with each other or store data in the cloud. In this class we will introduce you to Brillo and how NXP has worked with Google to bring Brillo to the i.MX 6UltraLite processor and other platforms. Watch Video Presentation
View full article
Advancing technology has brought down the cost of 24 GHz radar system significantly bringing a whole range of new applications into reach. Historically radar was a pure military and industrial application due to high application costs. With the latest generation of NXP BiCMOS technology this has changed. A 24 GHz radar frontend can now be fully integrated into a single IC bringing the costs and power dissipation down to consumer levels. This opens up a whole range of applications which were previously not possible. This lecture will show the possibilities of radar in different applications such as presence detection and consumer drone collision avoidance. A live demonstration based on first test chips in combination with ARM processors will be given.
View full article
This session explain how to achieve a higher level of security with NXP's latest NFC controller solution with customizable firmware, the PN7462, using a Secure Access Module (SAM) for applications like corporate access. The session follows the NFC access control hands-on workshop with a particular focus on security. In this session the PN7462 development kit will be used to demonstrate how high security using MIFARE DESFire EV1 and a SAM can be achieved.
View full article
By adding NFC to a door lock, the same smartcard technology that protects some of the world’s most valuable objects can now be brought to everyday places like homes, apartment buildings, and hotels. An NFC-enabled smartphone can be used to configure the lock, so homeowners can grant temporary access to a specific person or group. This hands-on session demonstrates how the latest NFC controller solution with customizable firmware, the PN7462, can be used for access applications. For the demonstration the PN7462 development kit will be used together with the software example to develop a door access application.
View full article
Embedded Planet designed the new NXP LS1043 Gateway. Come learn the details of the hardware and software designed for this next generation residential Gateway.
View full article
This session will provide a detailed introduction to NXP's HomeKit Software Development Kit (SDK) architecture, APIs and code adaptors. Through hands-on examples, you will learn accessory profile configurations, how to integrate with accessory application software, and how to build and debug a demo accessory (Restricted to verified MFi licensees only).
View full article
In designing cooking appliances, there is ample consideration given to power required from a home's wired electrical system as well as the performance needed to maintain safety and operating temperatures. NXP's solid state RF cooking team has partnered with Wayv Technology to develop a portable food heating appliance using solid state RF energy. This session will cover the key challenges and approaches to delivering energy to heat food in a portable, on-the-go appliance. Watch Video Presentation
View full article
There are many variables to consider when implementing and integrating solid state RF power into a cooking appliance. Cavity size and shape, RF feed type, power, thermals, and configuration all factor into design consideration. This session will cover key consideration and methods of simulating to achieve better system design. Watch Video Presentation
View full article
NXP introducing the most comprehensive smart home/IoT Evaluation kit enabling multiple technologies as wireless connectivity, security & NFC commissioning with audio features. NXP's complete value proposition combines to give best user experience, performance and accuracy to develop best home/building automation solutions.
View full article
Hands-on training for ZigBee-3.0 with NXP lowest power Wireless MCU, using evaluation kit. Quickest and fastest way to develop a smart home product using ZigBee-3.0 such as sensors, monitoring device panels, router devices and Gateway solutions.
View full article
Lecture on NFC commissioning and various use-cases NFC enables in Smart Home/IoT to save cost and enable convenience. NFC gives best of user experience for installing devices in Smart Home & Buildings and in-addition also useful for Diagnostic, de-commissioning, OTA upgrade and various other useful features.
View full article
This hands-on workshop provides a detailed architecture description of Thread technology and wireless mesh networking. The main Thread concepts will be reviewed and analyzed thoroughly. The attendee will have a deep understanding of the main concepts and how these are mapped to the NXP software API. The session will close with hands-on training to enable the attendee to understand software usage and configuration, low-power features and security concepts.
View full article
The Kinetis KE1x family is the next generation MCU solution in the Kinetis E series. Designed with more memory, enhanced features and new IPs, this family extends the NXP 5 V portfolio to cover higher performance applications and use cases. Together with the Kinetis KE0x family for entry level MCUs, the Kinetis E family becomes an ideal solution for markets needing 5 V, robustness, and more flash size, providing platform solutions for low-end to high-end applications. Join this session to learn how the strong EMC performance across the Kinetis E family makes it suitable for main control and HMI (touch) in home appliances, industrial, and other applications needed in harsh electrical noise environments. Watch Video Presentation
View full article