HMB-N1962 IPv6 Over Bluetooth® Low Energy (6LoBLE) Lecture and Demo
HMB-N1962 IPv6 Over Bluetooth® Low Energy (6LoBLE) Lecture and Demo
The course will detail RFC 7668 (6LoBLE), Bluetooth® low energy 4.2 and the Internet protocol support profile that are used to transport IPv6 frames in an IoT environment. The demo will be based on the Kinetis KW41 MCU.
Thanks for this Document. I really would like to implement this Demo on my own OpenWRT device to get a communication to each 6LN Node, which is connected to the 6LBR. So i'm interested in the slides 20 to 32. What I'm missing is a detailed description, which software hast to be implemented on the USB-KW41Z from the SDK_2.2_USB-KW41Z ? Which binary has to be implemented on the K22F on USB-KW41Z and which which HCI-example hast to be implemented on the KW41Z itself? On slide 21 is only mentioned that USB-KW41Z implements HCI App over UART! More detailed informations would be awesome! And which role, does the wireless_examples > bluetooth > ipv6router from the SDK, playing in this Demo!?