VisionSDK_S32V2 demo make error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

VisionSDK_S32V2 demo make error

1,977件の閲覧回数
17816877475
Contributor II

Hello everyone,

I have installed VisionSDK_S32V2_RTM_1_4_0 on my computer, and I want to build project with it  by make tool. So I watched the doc Vision SDK Programming Examples to see how to build an example. I select the most simplest example in /path/to/s32v234_sdk/demos/other/hello, but after I use make command,  the error occured!

Screenshot from 2019-10-15 14-26-35.png

My OS is Ubuntu16.04 64-bit, what's wrong with my operation? Any reply is OK.

I think my problem is the compiler, I have read the VisionSDK_UserGuide.pdf, whose chapter 3 describes the Build Environment, I have already add gcc-6.3.1-linaro-Earmv7-eabi/i686-linux/bin/ and gcc-6.3.1-linaro-Xarmv8-linux/i686-linux/bin to the PATH variable and setup the APU_TOOLS. But I don't how to set correct GNU GCC like below.

Screenshot from 2019-10-15 14-39-47.png

ywq,

2019.10.15

0 件の賞賛
返信
1 返信

1,874件の閲覧回数
bpe
NXP Employee
NXP Employee

Please be aware, that support to APEX, ISP and Vision SDK is currently provided via Tickets only. You will

receive a more detailed response by e-Mail, but for future requests regarding these features and related software,

please use only the link above.

Regards,

Platon.

0 件の賞賛
返信